Defines a platform abstraction layer for the Z-Wave power manager.

  • 2021 Silicon Laboratories Inc.

Modules#

pm_domain_status_t

Enumerations#

enum
ZPAL_PM_TYPE_USE_RADIO
ZPAL_PM_TYPE_USE_RADIO_TX = ZPAL_PM_TYPE_USE_RADIO
ZPAL_PM_TYPE_USE_RADIO_RX = ZPAL_PM_TYPE_USE_RADIO
ZPAL_PM_TYPE_DEEP_SLEEP
ZPAL_PM_TYPE_MAX
}

Power manager type in which a lock can request an opearation to prevent the system from entering a sleep mode.

enum
ZPAL_PM_ACTIVE
ZPAL_PM_LIGHT_SLEEP
ZPAL_PM_DEEP_SLEEP
ZPAL_PM_HALTED
}

Power manager power levels, each level corresponds to physical power mode implementation.

enum
ZPAL_PM_STATE_ACTIVE_PERMANENT
ZPAL_PM_STATE_ACTIVE_TIMER
ZPAL_PM_STATE_INACTIVE
ZPAL_PM_STATE_UNDEFINED
}

For each lock, three states are defined:

enum
ZPAL_PM_DOMAIN_APP
ZPAL_PM_DOMAIN_PAL
ZPAL_PM_DOMAIN_STACK
ZPAL_PM_DOMAIN_UNDEFINED
}

A domain is a group of locks.

Functions#

zpal_pm_lock(zpal_pm_type_t type, zpal_pm_domain_t domain, uint32_t timeout_ms, uint8_t idx)

Locks the power mode for a given time period.

zpal_pm_relock(zpal_pm_type_t type, zpal_pm_domain_t domain, uint32_t timeout_ms, uint8_t idx)

Locks the power mode for a given time period.

uint32_t

Gets the maximum timeout value that can be set for a lock.

bool
zpal_pm_lock_is_active(zpal_pm_type_t type, zpal_pm_domain_t domain, uint8_t idx, zpal_pm_state_t *state)

Return the state of a given lock.

bool
zpal_pm_lock_type_is_active(zpal_pm_type_t pm_type, zpal_pm_state_t *state)

Return the state of the given type of lock.

zpal_pm_register_domain(zpal_pm_domain_t domain, pm_domain_status_t *radio_domain_status, pm_domain_status_t *deep_sleep_domain_status)

Registers a domain for power locks.

zpal_pm_lock_cancel(zpal_pm_type_t type, zpal_pm_domain_t domain, uint8_t idx)

This function cancels an active power lock despite of the ongoing mode (permanent or timer).

void

Cancels all active power locks on both radio and deep sleep power locks.

void
zpal_zw_pm_event_handler(zpal_pm_powerlevel_t from, zpal_pm_powerlevel_t to)

Function to update stack logic (radio operations and configuration) before power mode transitions defined in zpal_pm_powerlevel_t.

void

Macro Definition Documentation#

ZPAL_PM_MAX_DOMAIN_LOCK_COUNT#

#define ZPAL_PM_MAX_DOMAIN_LOCK_COUNT
Value:
32

Enumeration Documentation#

zpal_pm_type_t#

zpal_pm_type_t

Power manager type in which a lock can request an opearation to prevent the system from entering a sleep mode.

Enumerator
ZPAL_PM_TYPE_USE_RADIO
ZPAL_PM_TYPE_USE_RADIO_TX
ZPAL_PM_TYPE_USE_RADIO_RX
ZPAL_PM_TYPE_DEEP_SLEEP
ZPAL_PM_TYPE_MAX

zpal_pm_powerlevel_t#

zpal_pm_powerlevel_t

Power manager power levels, each level corresponds to physical power mode implementation.

Enumerator
ZPAL_PM_ACTIVE

Processor is active.

ZPAL_PM_LIGHT_SLEEP

Processor is sleeping, but all peripherals are enabled.

ZPAL_PM_DEEP_SLEEP

Most peripherals are disabled, but the radio is in FLiRS mode.

ZPAL_PM_HALTED

Chip is off and will boot from reset. Hence, no transition from this power mode will ever happen.


zpal_pm_state_t#

zpal_pm_state_t

For each lock, three states are defined:

  • ZPAL_PM_STATE_ACTIVE_PERMANENT: The lock is active and will remain active until it is cancelled.

  • ZPAL_PM_STATE_ACTIVE_TIMER: The lock is active and will remain active until the timer expires.

  • ZPAL_PM_STATE_INACTIVE: The lock is inactive.

Enumerator
ZPAL_PM_STATE_ACTIVE_PERMANENT
ZPAL_PM_STATE_ACTIVE_TIMER
ZPAL_PM_STATE_INACTIVE
ZPAL_PM_STATE_UNDEFINED

zpal_pm_domain_t#

zpal_pm_domain_t

A domain is a group of locks.

They are stored in the same domain structure.

Enumerator
ZPAL_PM_DOMAIN_APP
ZPAL_PM_DOMAIN_PAL
ZPAL_PM_DOMAIN_STACK
ZPAL_PM_DOMAIN_UNDEFINED

Function Documentation#

zpal_pm_lock#

zpal_status_t zpal_pm_lock (zpal_pm_type_t type, zpal_pm_domain_t domain, uint32_t timeout_ms, uint8_t idx)

Locks the power mode for a given time period.

Parameters
TypeDirectionArgument NameDescription
zpal_pm_type_tN/Atype

The power manager type for the lock. If the lock is already active, this function does not overwrite the previous lock state. zpal_pm_relock can be used to overwrite the previous lock.

zpal_pm_domain_tN/Adomain

The domain in which the lock is registered.

uint32_tN/Atimeout_ms

The timeout duration in ms. If set to 0, the lock will be permanent. The maximum timeout value is defined by zpal_get_max_timeout.

uint8_tN/Aidx

The lock index

Returns

  • true when the lock is successfully acquired

  • ZPAL_STATUS_BUSY if the lock is already in active state.

  • ZPAL_STATUS_INVALID_ARGUMENT when the type or idx are invalid or timeout is greater than the maximum timeout.

  • ZPAL_STATUS_OK if the lock is successfully acquired.

Note


zpal_pm_relock#

zpal_status_t zpal_pm_relock (zpal_pm_type_t type, zpal_pm_domain_t domain, uint32_t timeout_ms, uint8_t idx)

Locks the power mode for a given time period.

Parameters
TypeDirectionArgument NameDescription
zpal_pm_type_tN/Atype

The power manager type for the lock.

zpal_pm_domain_tN/Adomain

The domain in which the lock is registered.

uint32_tN/Atimeout_ms

The timeout duration in ms. If set to 0, the lock will be permanent. The maximum timeout is return by zpal_get_max_timeout.

uint8_tN/Aidx

The lock index

If the lock is already active this function overwrites the previous lock. Use with caution. You can get the lock active state for the given id by calling zpal_pm_lock_is_activeReturns

  • true when the lock is successfully acquired, false otherwise (bad parameters).

  • ZPAL_STATUS_INVALID_ARGUMENT when the type or idx are invalid or timeout is greater than the maximum timeout.

  • ZPAL_STATUS_OK if the lock is successfully acquired.


zpal_get_max_timeout#

uint32_t zpal_get_max_timeout (void )

Gets the maximum timeout value that can be set for a lock.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • The maximum timeout value in ms.


zpal_pm_lock_is_active#

bool zpal_pm_lock_is_active (zpal_pm_type_t type, zpal_pm_domain_t domain, uint8_t idx, zpal_pm_state_t * state)

Return the state of a given lock.

Parameters
TypeDirectionArgument NameDescription
zpal_pm_type_t[in]type

The power manager type for the lock.

zpal_pm_domain_t[in]domain

The domain of the lock. A domain is a group of locks that can be managed together.

uint8_t[in]idx

The lock index

zpal_pm_state_t *[out]state

(otional) More detailed state of the lock: INACTIVE, ACTIVE_PERMANENT, ACTIVE_TIMER.

Returns

  • true is in active state, false if inactive.

Note


zpal_pm_lock_type_is_active#

bool zpal_pm_lock_type_is_active (zpal_pm_type_t pm_type, zpal_pm_state_t * state)

Return the state of the given type of lock.

Parameters
TypeDirectionArgument NameDescription
zpal_pm_type_t[in]pm_type

The power manager type to be checked.

zpal_pm_state_t *[out]state

(optional) More detailed state: INACTIVE, ACTIVE_PERMANENT, ACTIVE_TIMER.

Resulted from all zwave locks operations on that type. Returns

  • true if the lock is active, false if inactive.

Note

  • : Similar to zpal_pm_lock_is_active but done at the type level which contains any locks operating on that type.


zpal_pm_register_domain#

zpal_status_t zpal_pm_register_domain (zpal_pm_domain_t domain, pm_domain_status_t * radio_domain_status, pm_domain_status_t * deep_sleep_domain_status)

Registers a domain for power locks.

Parameters
TypeDirectionArgument NameDescription
zpal_pm_domain_tN/Adomain

The domain to be registered.

pm_domain_status_t *[in]radio_domain_status

Pointer to the radio domain status. If NULL, the domain will not be registered.

pm_domain_status_t *[in]deep_sleep_domain_status

Pointer to the deep sleep domain status. If NULL, the domain will not be registered.

Returns

  • ZPAL_STATUS_OK if one or two of the domains status are successfully registered, ZPAL_STATUS_FAIL otherwise.


zpal_pm_lock_cancel#

zpal_status_t zpal_pm_lock_cancel (zpal_pm_type_t type, zpal_pm_domain_t domain, uint8_t idx)

This function cancels an active power lock despite of the ongoing mode (permanent or timer).

Parameters
TypeDirectionArgument NameDescription
zpal_pm_type_t[in]type

The lock type to cancel.

zpal_pm_domain_tN/Adomain

The domain in which the lock is associated.

uint8_t[in]idx

The lock index to cancel.

Note

  • If the specified type is not supported, this function will not perform any action.

Returns

  • ZPAL_STATUS_OK if the lock is successfully cancelled, ZPAL_STATUS_FAIL otherwise.


zpal_pm_lock_cancel_all#

void zpal_pm_lock_cancel_all (void )

Cancels all active power locks on both radio and deep sleep power locks.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • It cancels all power locks created during runtime, hence it can be used ONLY as a part of power down routine.


zpal_zw_pm_event_handler#

void zpal_zw_pm_event_handler (zpal_pm_powerlevel_t from, zpal_pm_powerlevel_t to)

Function to update stack logic (radio operations and configuration) before power mode transitions defined in zpal_pm_powerlevel_t.

Parameters
TypeDirectionArgument NameDescription
zpal_pm_powerlevel_tN/Afrom

The power level from which the transition is happening.

zpal_pm_powerlevel_tN/Ato

The power level to which the transition is happening.

Note

  • This function is called through app_pm_transition_event and is mapped onto power manager platform specific events.


zpal_pm_halt#

void zpal_pm_halt (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A