Defines a platform abstraction layer for the Z-Wave radio.
2021 Silicon Laboratories Inc.
Modules#
zpal_radio_transmit_parameter_t
zpal_radio_transmit_parameter_t.__unnamed7__
Macros#
Opaque NVM payload size for Z-Wave IR calibration.
RSSI value is invalid or not measured.
Deprecateduse ZW_TX_POWER_100_DDBM instead
Deprecateduse ZW_TX_POWER_140_DDBM instead
Deprecateduse ZW_TX_POWER_200_DDBM instead
Number of channels of classic Z-Wave protocol.
Number of channels of Z-Wave Long Range protocol 100kbps, 40kbps, 9.6kbps and LRA/LRB (channel configuration 1 & 2)
LRA and LRB (channel configuration 3)
definition for maximum output power to use with zpal_tx_power_decidbm_t.
Number of 2 channel regions.
Number of 3 channel regions.
Enumerations#
Wakeup interval for the radio.
Enumeration containing supported checksum types in Z-Wave.
Enumeration containing supported baud rates.
Enumeration containing Long Range Channels.
Enumeration containing Z-Wave channels.
Enumeration containing Z-Wave channels known as protocol modes.
List of LR channel configuration.
Enumeration official Z-Wave regions.
Enumeration containing Tx power settings.
Z-Wave Frame header format types.
Receive radio events.
Transmit radio events.
Calibration radio events.
Typedefs#
Node ID type.
Parameter type to store deci dBm values.
Parameter type to store stay awake ids.
Function pointer declaration for handling of received frames.
Functions#
Sets the home ID & the node ID.
Initializes the radio hardware with the specified configuration profile.
Function used to change region and Long Range mode at the same time.
Function for getting REGION runtime.
Function for transmitting a Z-Wave frame though the radio.
Function for transmitting a Z-Wave Beam frame though the radio.
Starts the receiver and enables reception of frames.
Checks if data is available for processing in the radio module.
Restart the radio if a frame reception is in progress.
Function to get the last received frame.
Function to get the protocol mode used in the configured region.
Function for setting the LBT RSSI level.
Enable or disables reception of broadcast beam.
Function for clearing current Channel Transmit timers.
Function for clearing current Network statistics.
Returns the background RSSI (in dBm).
Function for getting the default tx power in deci dBm.
Puts the radio into an idle state.
Aborts any ongoing radio operation.
Shuts down the radio hardware.
Resets the radio configuration to receive mode after having received a beam.
Returns whether use of fragmented beams is enabled or not for the active region.
Returns whether listen before talk (LBT) is enabled.
Returns the time it takes to start transmission of wake up beams.
Returns the minimum transmit power for Z-Wave Long Range.
Returns the maximum transmit power for Z-Wave Long Range.
Disable the radio debug mode.
a getter on the current rf profile.
Function to read current Long Range Channel Configuration.
Function to read current Primary Long Range Channel.
Function to set the Primary Long Range Channel.
Function to read current Long Range Channel selection mode.
Function to set the Long Range Channel selction mode.
Function to check if the stack implementation supports a given region.
Check if transmission is allowed for specified channel.
Function to reduce Tx power of classic non-listening devices.
Return the maximum board supported tx power for classic z-wave.
Function to adjust the requested tx power for Long Range.
Function to radio calibration.
Run pending Radio calibrations (response to ZPAL_RADIO_EVENT_CAL_NEEDED).
Retrieves information about the last received beam.
Stores the average RSSI (Received Signal Strength Indicator) for a given Z-Wave channel.
Requests the radio to stay awake for a specified number of milliseconds.
Revokes a previous stay-awake request, allowing the radio to sleep as normal.
Lengthens the current stay-awake period.
Getter of wakeup state of the radio.
Registers a callback function to be invoked on radio state changes.
Inform the ZPAL radio layer that the node has been correctly included in a network.
Enumeration Documentation#
zpal_radio_listen_t#
zpal_radio_listen_t
Wakeup interval for the radio.
A FLiRS node will use 250 or 1000 ms interval, all other nodes should be configured as always listening.
| Enumerator | |
|---|---|
| ZPAL_RADIO_LISTEN_NEVER | Node is not listening (Only listen when application requests it). |
| ZPAL_RADIO_LISTEN_ALWAYS | Node is always listening. |
| ZPAL_RADIO_LISTEN_FREQUENTLY_250ms | Node wakes up every 250 ms interval to listen for a wakeup beam. |
| ZPAL_RADIO_LISTEN_FREQUENTLY_1000ms | Node wakes up every 1000 ms interval to listen for a wakeup beam. |
zpal_radio_crc_t#
zpal_radio_crc_t
Enumeration containing supported checksum types in Z-Wave.
| Enumerator | |
|---|---|
| ZPAL_RADIO_CRC_NONE | No checksum. |
| ZPAL_RADIO_CRC_8_BIT_XOR | 8 bit XOR checksum. |
| ZPAL_RADIO_CRC_16_BIT_CCITT | 16 bit CRC-CCITT checksum. |
zpal_radio_speed_t#
zpal_radio_speed_t
Enumeration containing supported baud rates.
| Enumerator | |
|---|---|
| ZPAL_RADIO_SPEED_UNDEFINED | |
| ZPAL_RADIO_SPEED_9600 | |
| ZPAL_RADIO_SPEED_40K | |
| ZPAL_RADIO_SPEED_100K | |
| ZPAL_RADIO_SPEED_100KLR | |
zpal_radio_lr_channel_t#
zpal_radio_lr_channel_t
Enumeration containing Long Range Channels.
| Enumerator | |
|---|---|
| ZPAL_RADIO_LR_CHANNEL_UNINITIALIZED | Long Range Channel setting not initialized. |
| ZPAL_RADIO_LR_CHANNEL_A | Long Range Channel A. |
| ZPAL_RADIO_LR_CHANNEL_B | Long Range Channel B. |
| ZPAL_RADIO_LR_CHANNEL_UNKNOWN | Long Range Channel Unknown. |
| ZPAL_RADIO_LR_CHANNEL_AUTO | Long Range automatically selected Channel. |
zpal_radio_zwave_channel_t#
zpal_radio_zwave_channel_t
Enumeration containing Z-Wave channels.
| Enumerator | |
|---|---|
| ZPAL_RADIO_ZWAVE_CHANNEL_0 | Z-Wave channel 0. |
| ZPAL_RADIO_ZWAVE_CHANNEL_1 | Z-Wave channel 1. |
| ZPAL_RADIO_ZWAVE_CHANNEL_2 | Z-Wave channel 2. |
| ZPAL_RADIO_ZWAVE_CHANNEL_3 | Z-Wave channel 3. |
| ZPAL_RADIO_ZWAVE_CHANNEL_4 | Z-Wave channel 4. |
| ZPAL_RADIO_ZWAVE_CHANNEL_NUM | Number of Z-Wave channels. must be last. |
| ZPAL_RADIO_ZWAVE_CHANNEL_UNKNOWN | Z-Wave channel Unknown. |
zpal_radio_protocol_mode_t#
zpal_radio_protocol_mode_t
Enumeration containing Z-Wave channels known as protocol modes.
| Enumerator | |
|---|---|
| ZPAL_RADIO_PROTOCOL_MODE_1 | 2 Channel Protocol Mode. |
| ZPAL_RADIO_PROTOCOL_MODE_2 | 3 Channel Protocol Mode. |
| ZPAL_RADIO_PROTOCOL_MODE_3 | 4 Channel Protocol Mode - Combination of 2 Channel (9.6kb/40kb, 100kb) and Long Range Channel. |
| ZPAL_RADIO_PROTOCOL_MODE_4 | 2 Long Range Channel Protocol Mode - End Device. |
| ZPAL_RADIO_PROTOCOL_MODE_UNDEFINED | Protocol mode undefined means invalid region code. |
zpal_radio_lr_channel_config_t#
zpal_radio_lr_channel_config_t
List of LR channel configuration.
Used to select the correct phy configuration.
| Enumerator | |
|---|---|
| ZPAL_RADIO_LR_CH_CFG_NO_LR | used if region does not support Long range or end device included in classic network. |
| ZPAL_RADIO_LR_CH_CFG1 | used by controller with primary channel A and not included end device Phy is configured to listen on classic Z-Wave channels and Long Range channel A. |
| ZPAL_RADIO_LR_CH_CFG2 | used only by controller with primary channel B Phy is configured to listen on classic Z-Wave channels and Long Range channel B. |
| ZPAL_RADIO_LR_CH_CFG3 | used only by end device when included in a LR network. |
| ZPAL_RADIO_LR_CH_CFG_COUNT | enumeration items count |
zpal_radio_region_t#
zpal_radio_region_t
Enumeration official Z-Wave regions.
| Enumerator | |
|---|---|
| REGION_2CH_FIRST | First 2 channels region (with 3 data rates) |
| REGION_EU | Radio is located in Region EU. 2 Channel region. |
| REGION_US | Radio is located in Region US. 2 Channel region. |
| REGION_ANZ | Radio is located in Region Australia/New Zealand. 2 Channel region. |
| REGION_HK | Radio is located in Region Hong Kong. 2 Channel region. |
| REGION_DEPRECATED_4 | Deprecated value, should never be used. |
| REGION_IN | Radio is located in Region India. 2 Channel region. |
| REGION_IL | Radio is located in Region Israel. 2 Channel region. |
| REGION_RU | Radio is located in Region Russia. 2 Channel region. |
| REGION_CN | Radio is located in Region China. 2 Channel region. |
| REGION_US_LR | Radio is located in Region US. 2 Channel LR region. |
| REGION_DEPRECATED_10 | Deprecated value, should never be used. |
| REGION_EU_LR | Radio is located in Region EU. 2 Channel LR region. |
| REGION_2CH_END | end of 2 channels regions (with 3 data rates) |
| REGION_3CH_FIRST | First 3 channels region (with 1 data rate) |
| REGION_JP | Radio is located in Region Japan. 3 Channel region. |
| REGION_KR | Radio is located in Region Korea. 3 Channel region. |
| REGION_3CH_END | end of 3 channels regions (with 1 data rate) |
| REGION_DEPRECATED_48 | Deprecated value, should never be used. |
| REGION_UNDEFINED | |
| REGION_DEFAULT | Radio is located in Library Default Region EU. 2 Channel region. |
zpal_radio_tx_power_t#
zpal_radio_tx_power_t
Enumeration containing Tx power settings.
| Enumerator | |
|---|---|
| ZPAL_RADIO_TX_POWER_DEFAULT | Max Tx power. |
| ZPAL_RADIO_TX_POWER_MINUS1_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS2_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS3_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS4_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS5_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS6_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS7_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS8_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS9_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS10_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS11_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS12_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS13_DBM | |
| ZPAL_RADIO_TX_POWER_MINUS14_DBM | |
| ZPAL_RADIO_TX_POWER_REDUCED | Default reduced Tx power. |
zpal_radio_header_type_t#
zpal_radio_header_type_t
Z-Wave Frame header format types.
| Enumerator | |
|---|---|
| ZPAL_RADIO_HEADER_TYPE_2CH | 2 Channel header format. |
| ZPAL_RADIO_HEADER_TYPE_3CH | 3 Channel header format. |
| ZPAL_RADIO_HEADER_TYPE_LR | LR Channel header format. |
| ZPAL_RADIO_HEADER_TYPE_UNDEFINED | Undefined Channel header format. |
zpal_radio_rx_event_t#
zpal_radio_rx_event_t
Receive radio events.
| Enumerator | |
|---|---|
| ZPAL_RADIO_EVENT_RX_COMPLETE | Frame received. |
| ZPAL_RADIO_EVENT_RX_BEAM_COMPLETE | Beam received. |
| ZPAL_RADIO_EVENT_RX_ABORT | Receive was aborted. |
zpal_radio_tx_event_t#
zpal_radio_tx_event_t
Transmit radio events.
| Enumerator | |
|---|---|
| ZPAL_RADIO_EVENT_TX_COMPLETE | Transmit complete. |
| ZPAL_RADIO_EVENT_TX_BEAM_COMPLETE | Beam sent. |
| ZPAL_RADIO_EVENT_TX_FAIL | Transmit failed. |
| ZPAL_RADIO_EVENT_TX_FAIL_LBT | Transmit failed because of an LBT failure. |
| ZPAL_RADIO_EVENT_TX_NONE | No transmit event. |
zpal_radio_cal_event_t#
zpal_radio_cal_event_t
Calibration radio events.
| Enumerator | |
|---|---|
| ZPAL_RADIO_EVENT_CAL_NEEDED | Radio needs calibration; stack shall call zpal_radio_calibrate(). |
| ZPAL_RADIO_EVENT_IR_CAL_COMPLETE | IR calibration complete; stack shall persist calibration data. |
zpal_radio_application_t#
zpal_radio_application_t
| Enumerator | |
|---|---|
| ZPAL_RADIO_APPLICATION_CONTROLLER | Controller mode. |
| ZPAL_RADIO_APPLICATION_END_DEVICE | End Device mode. |
| ZPAL_RADIO_APPLICATION_ZNIFFER | Zniffer mode. |
zpal_radio_status_t#
zpal_radio_status_t
| Enumerator | |
|---|---|
| ZPAL_RADIO_STATUS_OFF | Radio is off. |
| ZPAL_RADIO_STATUS_FLIRS | Radio is in Beam receive mode. |
| ZPAL_RADIO_STATUS_ON | Radio is in normal operating mode. |
Typedef Documentation#
zpal_tx_power_decidbm_t#
typedef int16_t zpal_tx_power_decidbm_t
Parameter type to store deci dBm values.
zpal_tx_power_t#
typedef zpal_tx_power_decidbm_t zpal_tx_power_t
Deprecateduse zpal_tx_power_decidbm_t instead
zpal_radio_stay_awake_id_t#
typedef uint32_t zpal_radio_stay_awake_id_t
Parameter type to store stay awake ids.
zpal_radio_rx_callback_t#
typedef void(* zpal_radio_rx_callback_t) (zpal_radio_rx_event_t event) )(zpal_radio_rx_event_t event)
zpal_radio_tx_callback_t#
typedef void(* zpal_radio_tx_callback_t) (zpal_radio_tx_event_t event) )(zpal_radio_tx_event_t event)
zpal_radio_cal_callback_t#
typedef void(* zpal_radio_cal_callback_t) (zpal_radio_cal_event_t event) )(zpal_radio_cal_event_t event)
zpal_radio_region_change_callback_t#
typedef void(* zpal_radio_region_change_callback_t) (void) )(void)
zpal_radio_receive_handler_t#
typedef void(* zpal_radio_receive_handler_t) (zpal_radio_rx_parameters_t *rx_parameters, zpal_radio_receive_frame_t *frame) )(zpal_radio_rx_parameters_t *rx_parameters, zpal_radio_receive_frame_t *frame)
Function pointer declaration for handling of received frames.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | rx_parameters | Pointer to the structure with channel and rssi values. | |
| [in] | frame | Pointer to the received frame. The frame is expected to be located in Z-Wave stack reserved memory and allocated throughout lifetime of stack processing. Application should copy payload data if required for unsynchronized data processing. |
When a frame is received this function will be invoked in order to process the frame.
zpal_radio_status_callback_t#
typedef void(* zpal_radio_status_callback_t) (const zpal_radio_status_t state) )(const zpal_radio_status_t state)
Function Documentation#
zpal_radio_set_network_ids#
void zpal_radio_set_network_ids (uint32_t home_id, node_id_t node_id, uint8_t home_id_hash)
Sets the home ID & the node ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | home_id | Network home ID. |
| node_id_t | [in] | node_id | Network node ID. |
| uint8_t | [in] | home_id_hash | HomeID Hash. Used only for Flirs. |
zpal_radio_init#
zpal_status_t zpal_radio_init (const zpal_radio_profile_t *const profile)
Initializes the radio hardware with the specified configuration profile.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const zpal_radio_profile_t *const | [in] | profile | Pointer to a structure containing the configuration parameters for the radio. This must be properly initialized before calling this function. |
This function sets up the radio module based on the provided profile, ensuring it is ready for operation. The profile contains necessary configuration parameters such as frequency, and other radio-specific settings.
Note
Ensure that the profile is valid and all required fields are set before invoking this function to avoid undefined behavior.
Returns
ZPAL_STATUS_OK if the zpal radio layer is ready. ZPAL_STATUS_INVALID_ARGUMENT if
profileis NULL orprofile->cal_cfg.datais NULL.
zpal_radio_change_region#
zpal_status_t zpal_radio_change_region (zpal_radio_region_t eRegion, zpal_radio_lr_channel_config_t eLrChCfg)
Function used to change region and Long Range mode at the same time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_region_t | [in] | eRegion | Region to change to. |
| zpal_radio_lr_channel_config_t | [in] | eLrChCfg | long range mode to change to (in case of no LR region, should be set to ZPAL_RADIO_LR_CH_CFG_NO_LR). |
Returns
ZPAL_STATUS_OK if the region was successfully changed and ZPAL_STATUS_FAIL otherwise.
zpal_radio_get_region#
zpal_radio_region_t zpal_radio_get_region (void )
Function for getting REGION runtime.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Current region.
zpal_radio_transmit#
zpal_status_t zpal_radio_transmit (zpal_radio_transmit_parameter_t const *const tx_parameters, uint8_t frame_header_length, uint8_t const *const frame_header_buffer, uint8_t frame_payload_length, uint8_t const *const frame_payload_buffer, uint8_t is_retransmission)
Function for transmitting a Z-Wave frame though the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_transmit_parameter_t const *const | [in] | tx_parameters | Parameter setting specifying speed, channel, wakeup, crc for transmission. |
| uint8_t | [in] | frame_header_length | Length of frame header data to transmit. |
| uint8_t const *const | [in] | frame_header_buffer | Pointer to data array containing the frame header. |
| uint8_t | [in] | frame_payload_length | Length of frame payload data to transmit. |
| uint8_t const *const | [in] | frame_payload_buffer | Pointer to data array containing the frame payload. |
| uint8_t | N/A | is_retransmission |
Returns
ZPAL_STATUS_OK if the data was successfully transmit, ZPAL_STATUS_BUFFER_FULL when queue is full.
zpal_radio_transmit_beam#
zpal_status_t zpal_radio_transmit_beam (zpal_radio_transmit_parameter_t const *const tx_parameters, uint8_t beam_data_len, uint8_t const *const beam_data)
Function for transmitting a Z-Wave Beam frame though the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_transmit_parameter_t const *const | [in] | tx_parameters | Parameter setting specifying speed, channel, wakeup. |
| uint8_t | [in] | beam_data_len | Length of the Beam data to transmit. |
| uint8_t const *const | [in] | beam_data | Pointer to data array containing the BEAM data. |
Returns
ZPAL_STATUS_OK if the data was successfully transmit, ZPAL_STATUS_BUFFER_FULL when queue is full, ZPAL_STATUS_INVALID_ARGUMENT if
beam_data_lenis too large orrepeatsis 0.
zpal_radio_start_receive#
zpal_status_t zpal_radio_start_receive (void )
Starts the receiver and enables reception of frames.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
If the receiver is already started, nothing will happen.
zpal_radio_is_data_available#
bool zpal_radio_is_data_available (void )
Checks if data is available for processing in the radio module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function determines whether there is any data available in the radio module that can be processed or retrieved.
Returns
True if data is available, false otherwise.
zpal_radio_restart_if_rx_in_progress#
zpal_status_t zpal_radio_restart_if_rx_in_progress (void )
Restart the radio if a frame reception is in progress.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The radio is restarted once the frame is completed.
If a frame reception is in progress, the function wait for the end of the frame then restart the radio (in Rx mode). In other case, the function does nothing
Returns
ZPAL_STATUS_OK if the radio ready in receiver mode ZPAL_STATUS_BUSY if the radio is not in Rx. ZPAL_STATUS_FAIL if the function has failed to restart the radio
zpal_radio_get_last_received_frame#
zpal_status_t zpal_radio_get_last_received_frame (zpal_radio_receive_frame_t * frame)
Function to get the last received frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_receive_frame_t * | [out] | frame | Pointer to a structure where the last received frame will be stored. |
This function retrieves the oldest received Z-Wave frame from the radio module. The frame data is stored in the provided structure.
Returns
ZPAL_STATUS_OK if a valid frame is available and retrieved. ZPAL_STATUS_FAIL if no frame is available or an error occurred.
zpal_radio_get_protocol_mode#
zpal_radio_protocol_mode_t zpal_radio_get_protocol_mode (void )
Function to get the protocol mode used in the configured region.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Protocol mode used in the configured region.
zpal_radio_set_lbt_level#
void zpal_radio_set_lbt_level (uint8_t channel, int8_t level)
Function for setting the LBT RSSI level.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel | uint8_t channel to set LBT threshold for. |
| int8_t | [in] | level | int8_t LBT RSSI level in dBm. |
zpal_radio_enable_rx_broadcast_beam#
void zpal_radio_enable_rx_broadcast_beam (bool enable)
Enable or disables reception of broadcast beam.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | true to enable FLiRS broadcast address, false to disable. |
Enable or disable FLiRS broadcast address.
zpal_radio_clear_tx_timers#
void zpal_radio_clear_tx_timers (void )
Function for clearing current Channel Transmit timers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
zpal_radio_clear_network_stats#
void zpal_radio_clear_network_stats (void )
Function for clearing current Network statistics.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
zpal_radio_get_background_rssi#
zpal_status_t zpal_radio_get_background_rssi (uint8_t channel, int8_t * rssi)
Returns the background RSSI (in dBm).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel | uint8_t channel Id for measurement. |
| int8_t * | [out] | rssi | pointer where to store the background RSSI value. |
Returns
ZPAL_STATUS_OK if a valid RSSI value is available and read. ZPAL_STATUS_BUSY if the radio is busy (TX/RX active), or if the underlying RAIL channel-hopping RSSI read is invalid. In those cases rssi is set to SL_RAIL_RSSI_INVALID_DBM. ZPAL_STATUS_INVALID_ARGUMENT if rssi pointer is null.
zpal_radio_get_default_tx_power#
zpal_tx_power_decidbm_t zpal_radio_get_default_tx_power (void )
Function for getting the default tx power in deci dBm.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The default RF TX power in deci dBm
zpal_radio_idle#
zpal_status_t zpal_radio_idle (void )
Puts the radio into an idle state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function transitions the radio to an idle state where it is neither transmitting nor receiving. It can be used to conserve power or prepare the radio for a new operation.
zpal_radio_abort#
zpal_status_t zpal_radio_abort (void )
Aborts any ongoing radio operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function halts any current transmission or reception activity and brings the radio to an idle state. It can be used to immediately stop the radio's operation in case of an error or when a higher-priority operation needs to be performed.
zpal_radio_shutdown#
zpal_status_t zpal_radio_shutdown (void )
Shuts down the radio hardware.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function powers down the radio hardware, ensuring it is in a low-power state. It should be called when the radio is no longer needed to conserve energy.
Note
This function is definitive and should be used with caution. Once called, the radio cannot be restarted without reinitializing it.
zpal_radio_reset_after_beam_receive#
zpal_status_t zpal_radio_reset_after_beam_receive (bool start_receiver)
Resets the radio configuration to receive mode after having received a beam.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | start_receiver | If set to true, the receiver will start listening. Otherwise, it will stay inactive. |
zpal_radio_is_fragmented_beam_enabled#
bool zpal_radio_is_fragmented_beam_enabled (void )
Returns whether use of fragmented beams is enabled or not for the active region.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
True if use of fragmented beams is enabled, false otherwise.
zpal_radio_is_lbt_enabled#
bool zpal_radio_is_lbt_enabled (void )
Returns whether listen before talk (LBT) is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
True if LBT is enabled, false otherwise.
zpal_radio_get_beam_startup_time#
uint16_t zpal_radio_get_beam_startup_time (void )
Returns the time it takes to start transmission of wake up beams.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Includes time spent on LBT.
Returns
startup time in milli seconds.
zpal_radio_get_minimum_lr_tx_power#
zpal_tx_power_decidbm_t zpal_radio_get_minimum_lr_tx_power (void )
Returns the minimum transmit power for Z-Wave Long Range.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Minimum TX power in deci dBm.
zpal_radio_get_maximum_lr_tx_power#
zpal_tx_power_decidbm_t zpal_radio_get_maximum_lr_tx_power (void )
Returns the maximum transmit power for Z-Wave Long Range.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Maximum TX power in deci dBm.
zpal_radio_disable_debug#
zpal_status_t zpal_radio_disable_debug (void )
Disable the radio debug mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function disables the radio debug mode
zpal_radio_get_rf_profile#
const zpal_radio_profile_t * zpal_radio_get_rf_profile (void )
a getter on the current rf profile.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Function return a pointer (instead of a struct) to reduce RAM memory usage and execution time. The pointer target a const structure because it should not be used to modify the content of the structure.
Returns
pointer on the current rf profile.
zpal_radio_get_lr_channel_config#
zpal_radio_lr_channel_config_t zpal_radio_get_lr_channel_config (void )
Function to read current Long Range Channel Configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
current long rang channel configuration (ZPAL_RADIO_LR_Ch_CFG if region without lr)
zpal_radio_get_primary_long_range_channel#
zpal_radio_lr_channel_t zpal_radio_get_primary_long_range_channel (void )
Function to read current Primary Long Range Channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
zpal_radio_set_primary_long_range_channel#
void zpal_radio_set_primary_long_range_channel (zpal_radio_lr_channel_t channel)
Function to set the Primary Long Range Channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_lr_channel_t | [in] | channel | zpal_radio_lr_channel_t Long Range Channel to set as Primary Long Range Channel. |
zpal_radio_get_long_range_channel_auto_mode#
bool zpal_radio_get_long_range_channel_auto_mode (void )
Function to read current Long Range Channel selection mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true for automatically slected channel, false for manually selected channel
zpal_radio_set_long_range_channel_auto_mode#
zpal_status_t zpal_radio_set_long_range_channel_auto_mode (bool enable)
Function to set the Long Range Channel selction mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | true to enable the automatically channel selection mode, false to enable the manual channel selection mode |
Returns
ZPAL_STATUS_OK if the mode was successfully set, ZPAL_STATUS_FAIL otherwise.
zpal_radio_is_region_supported#
bool zpal_radio_is_region_supported (zpal_radio_region_t region)
Function to check if the stack implementation supports a given region.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_region_t | [in] | region | Region to check |
Returns
True if the region is supported, False if it is not
zpal_radio_is_transmit_allowed#
bool zpal_radio_is_transmit_allowed (uint8_t channel, uint8_t frame_length, bool cca)
Check if transmission is allowed for specified channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | channel | The channel to check. |
| uint8_t | [in] | frame_length | The length of the frame to send. |
| bool | [in] | cca | If true, the function will provision cca_duration into transmission time. |
Returns
True if node shall use Long Range channel only.
zpal_radio_attenuate#
bool zpal_radio_attenuate (zpal_radio_tx_power_t adjust_tx_power)
Function to reduce Tx power of classic non-listening devices.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_tx_power_t | [in] | adjust_tx_power | Reduces the devices default Tx power in dB. Valid range: 0-9 dB. |
Returns
True when reduction is allowed, false for listening devices and out of range input.
zpal_radio_get_maximum_tx_power#
zpal_tx_power_decidbm_t zpal_radio_get_maximum_tx_power (void )
Return the maximum board supported tx power for classic z-wave.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The maximum board supported tx power in deci dBm.
zpal_radio_limit_lr_power_to_capability#
zpal_tx_power_decidbm_t zpal_radio_limit_lr_power_to_capability (zpal_tx_power_decidbm_t requested_power)
Function to adjust the requested tx power for Long Range.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_tx_power_decidbm_t | [in] | requested_power | The requested tx power in deci dBm. |
This function ensures that the requested power is within the allowed range
Returns
The adjusted tx power in deci dBm.
zpal_radio_request_calibration#
void zpal_radio_request_calibration (bool forced)
Function to radio calibration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | forced | If true, radio calibration is performed regardless if it is required. If false, radio calibration is performed only if it is required. |
zpal_radio_calibrate#
zpal_status_t zpal_radio_calibrate (void )
Run pending Radio calibrations (response to ZPAL_RADIO_EVENT_CAL_NEEDED).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
ZPAL_STATUS_OK on success, ZPAL_STATUS_FAIL on error.
zpal_radio_get_last_beam_info#
zpal_status_t zpal_radio_get_last_beam_info (zpal_radio_beam_info_t * beamInfo)
Retrieves information about the last received beam.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_beam_info_t * | [out] | beamInfo | Pointer to the structure where the beam information will be stored. |
Returns
ZPAL_STATUS_OK if the beam information was successfully retrieved, ZPAL_STATUS_INVALID_ARGUMENT if beamInfo is NULL.
zpal_radio_rf_channel_statistic_store_background_rssi_average#
void zpal_radio_rf_channel_statistic_store_background_rssi_average (zpal_radio_zwave_channel_t zwavechannel, int8_t averagerssi)
Stores the average RSSI (Received Signal Strength Indicator) for a given Z-Wave channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_zwave_channel_t | N/A | zwavechannel | The Z-Wave channel for which the RSSI average is to be calculated. |
| int8_t | N/A | averagerssi | The average RSSI value to be used for the calculation. |
This function stores the background RSSI average for the specified Z-Wave channel.
zpal_radio_request_stay_awake#
zpal_status_t zpal_radio_request_stay_awake (uint32_t msecs, zpal_radio_stay_awake_id_t * id)
Requests the radio to stay awake for a specified number of milliseconds.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | msecs | Number of millisecs to stay awake (ZPAL_RADIO_STAY_AWAKE_ALWAYS = never ends). |
| zpal_radio_stay_awake_id_t * | N/A | id | Pointer to a variable where the identifier for the stay-awake request will be stored. This identifier is used to revoke the request later. NULL value is accepted, but it won't be possible to revoke the request later. |
Returns
ZPAL_STATUS_OK if the request was successful, ZPAL_STATUS_INVALID_ARGUMENT if the duration exceeds the maximum supported value or another error occurs.
Note
Duration Limit: Maximum duration is limited by INT32_MAX ticks in the underlying sleeptimer. The actual maximum milliseconds depends on the platform's sleeptimer frequency. At the default 32768 Hz, this is approximately 18.2 hours (1,092,266 ms). Requests exceeding this limit will fail. For indefinite duration, use ZPAL_RADIO_STAY_AWAKE_ALWAYS instead.
Timer Synchronization: This API uses platform-specific timers (hardware-based on Silicon Labs). When combining with OS-level timers (e.g., FreeRTOS ctimer), ensure stay_awake duration exceeds the OS timeout to account for scheduler latency. Example: if ctimer fires at 240ms, set stay_awake to 440ms (240 + 200ms margin). This prevents device to shutoff radio and eventually sleep before callback execution on low-power devices.
zpal_radio_revoke_stay_awake#
zpal_status_t zpal_radio_revoke_stay_awake (zpal_radio_stay_awake_id_t * id)
Revokes a previous stay-awake request, allowing the radio to sleep as normal.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_stay_awake_id_t * | N/A | id | Pointer to the identifier of the stay-awake request to revoke. NULL is used as a special value to revoke permanent stay-awake requests. |
Note
The pointer to the identifier is set to 0 after revocation.
Radio will transition to off or flirs mode if there are no other active stay-awake requests.
zpal_radio_update_stay_awake#
zpal_status_t zpal_radio_update_stay_awake (zpal_radio_stay_awake_id_t * id, uint32_t new_msecs)
Lengthens the current stay-awake period.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_stay_awake_id_t * | N/A | id | Pointer to the identifier of the stay-awake request to update. |
| uint32_t | N/A | new_msecs | The new length (in millisecs) to request from now. |
Returns
ZPAL_STATUS_OK if the request was successful, ZPAL_STATUS_INVALID_ARGUMENT if the duration exceeds the maximum supported value or another error occurs.
Note
Duration Limit: Maximum duration is limited by INT32_MAX ticks in the underlying sleeptimer. See zpal_radio_request_stay_awake() for details.
This function is equivalent to revoking the previous request and creating a new one.
zpal_radio_get_wakeup_status#
zpal_radio_status_t zpal_radio_get_wakeup_status (void )
Getter of wakeup state of the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Current wakeup state of the radio
zpal_radio_set_status_callback#
zpal_status_t zpal_radio_set_status_callback (zpal_radio_status_callback_t callback)
Registers a callback function to be invoked on radio state changes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| zpal_radio_status_callback_t | [in] | callback | The function pointer to the callback to be registered. Pass NULL to unregister the current callback. |
This function sets the callback that will be called whenever the radio state changes. The callback function should match the signature defined by zpal_radio_state_callback_t.
Returns
zpal_status_t Returns status code indicating success or failure of the operation.
zpal_radio_set_joinable#
zpal_status_t zpal_radio_set_joinable (bool is_joinable)
Inform the ZPAL radio layer that the node has been correctly included in a network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | is_joinable | true if the node has been correctly included, false otherwise. |
Correctly included means that the node is joinable with tuple (homeid, nodeid).
Returns
zpal_status_t Returns status code indicating success or failure of the operation. ZPAL_STATUS_OK if the operation was successful.