Cluster Commands: Device Management
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CHG_OF_TENANCY |
zcl dm get-chg-of-tenancy | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CHG_OF_SUPPLIER |
zcl dm get-chg-of-supplier | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_REQ_NEW_PASS |
zcl dm req-new-pass [passwordType:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_SITE_ID |
zcl dm get-site-id | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_RPT_EVENT_CONFIG |
zcl dm rpt-event-config [commandIndex:1] [totalCommands:1] [eventConfigurationPayload:3] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CIN |
zcl dm get-cin | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_PUB_CHG_OF_SUPPLIER |
zcl dm pub-chg-of-supplier [currentProviderId:4] [issuerEventId:4] [tariffType:1] [proposedProviderId:4] [providerChangeImplementationTime:4] [providerChangeControl:4] [proposedProviderName:-1] [proposedProviderContactDetails:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_REQ_NEW_PASS_RESP |
zcl dm req-new-pass-resp [issuerEventId:4] [implementationDateTime:4] [durationInMinutes:2] [passwordType:1] [password:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_SET_EVENT_CONFIG |
zcl dm set-event-config [issuerEventId:4] [startDateTime:4] [eventConfiguration:1] [configurationControl:1] [eventConfigurationPayload:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_EVENT_CONFIG |
zcl dm get-event-config [eventId:2] |
Detailed Description
This group describes the CLI commands for the Device Management cluster. Listed below is a description of the cluster:
This cluster provides attributes and commands to support device-cognisant application layer protocols.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CHG_OF_SUPPLIER |
zcl dm get-chg-of-supplier
- This command is used to request the ESI to respond with information regarding any available change of supplier.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CHG_OF_TENANCY |
zcl dm get-chg-of-tenancy
- This command is used to request the ESI to respond with information regarding any available change of tenancy.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_CIN |
zcl dm get-cin
- This command is used to request the ESI to respond with information regarding any pending change of Customer ID Number.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_EVENT_CONFIG |
zcl dm get-event-config [eventId:2]
- This command allows the server to request details of event configurations.
- eventId - INT16U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_GET_SITE_ID |
zcl dm get-site-id
- This command is used to request the ESI to respond with information regarding any pending change of Site ID.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_PUB_CHG_OF_SUPPLIER |
zcl dm pub-chg-of-supplier [currentProviderId:4] [issuerEventId:4] [tariffType:1] [proposedProviderId:4] [providerChangeImplementationTime:4] [providerChangeControl:4] [proposedProviderName:-1] [proposedProviderContactDetails:-1]
- This command is used to change the Supplier (energy supplier) that is supplying the meter (s).
- currentProviderId - INT32U
- issuerEventId - INT32U
- tariffType - TariffType [ENUM8]
- proposedProviderId - INT32U
- providerChangeImplementationTime - UTC_TIME
- providerChangeControl - ProposedChangeControl [BITMAP32]
- proposedProviderName - OCTET_STRING
- proposedProviderContactDetails - OCTET_STRING
- See also
- EmberAfTariffType
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_REQ_NEW_PASS |
zcl dm req-new-pass [passwordType:1]
- This command is used to request the current password from the server.
- passwordType - PasswordType [ENUM8]
- See also
- EmberAfPasswordType
- passwordType - PasswordType [ENUM8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_REQ_NEW_PASS_RESP |
zcl dm req-new-pass-resp [issuerEventId:4] [implementationDateTime:4] [durationInMinutes:2] [passwordType:1] [password:-1]
- This command is used to send the current password to the client.
- issuerEventId - INT32U
- implementationDateTime - UTC_TIME
- durationInMinutes - INT16U
- passwordType - PasswordType [ENUM8]
- password - OCTET_STRING
- See also
- EmberAfPasswordType
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_RPT_EVENT_CONFIG |
zcl dm rpt-event-config [commandIndex:1] [totalCommands:1] [eventConfigurationPayload:3]
- This command is sent in response to a GetEventConfiguration command.
- commandIndex - INT8U
- totalCommands - INT8U
- eventConfigurationPayload - struct EventConfigurationPayload
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DEVICE_MANAGEMENT_SET_EVENT_CONFIG |
zcl dm set-event-config [issuerEventId:4] [startDateTime:4] [eventConfiguration:1] [configurationControl:1] [eventConfigurationPayload:1]
- This command provides a method to set the event configuration attributes, held in a client device.
- issuerEventId - INT32U
- startDateTime - UTC_TIME
- eventConfiguration - EventConfiguration [BITMAP8]
- configurationControl - EventConfigurationControl [ENUM8]
- eventConfigurationPayload - INT8U
- See also
- EmberAfEventConfigurationControl