Cluster Commands: Events
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_EVENTS_GET_EVENT_LOG |
zcl events get-event-log [eventControlLogId:1] [eventId:2] [startTime:4] [endTime:4] [numberOfEvents:1] [eventOffset:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_EVENTS_CLEAR_EVENT_LOG |
zcl events clear-event-log [logId:1] |
Detailed Description
This group describes the CLI commands for the Events cluster. Listed below is a description of the cluster:
This cluster provides an interface on which applications can use event-based protocols.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_EVENTS_CLEAR_EVENT_LOG |
zcl events clear-event-log [logId:1]
- The ClearEventLogRequest command requests that an Events server device clear the specified event log(s).
- logId - EventLogId [ENUM8]
- See also
- EmberAfEventLogId
- logId - EventLogId [ENUM8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_EVENTS_GET_EVENT_LOG |
zcl events get-event-log [eventControlLogId:1] [eventId:2] [startTime:4] [endTime:4] [numberOfEvents:1] [eventOffset:2]
- The GetEventLog command allows a client to request events from a server's event logs. One or more PublishEventLog commands are returned on receipt of this command.
- eventControlLogId - EventControlLogId [BITMAP8]
- eventId - INT16U
- startTime - UTC_TIME
- endTime - UTC_TIME
- numberOfEvents - INT8U
- eventOffset - INT16U