Zigbee PRO Library EZSP Command Handlers Callbacks

Functions

EmberStatus emberAfPluginEzspZigbeeProSetConcentratorCommandCallback (bool on, uint16_t concentratorType, uint16_t minTime, uint16_t maxTime, uint8_t routeErrorThreshold, uint8_t deliveryFailureThreshold, uint8_t maxHops)

Detailed Description

These callbacks are contributed by the Zigbee PRO Library EZSP Command Handlers plugin.

Function Documentation

EmberStatus emberAfPluginEzspZigbeeProSetConcentratorCommandCallback ( bool  on,
uint16_t  concentratorType,
uint16_t  minTime,
uint16_t  maxTime,
uint8_t  routeErrorThreshold,
uint8_t  deliveryFailureThreshold,
uint8_t  maxHops 
)

References EMBER_INVALID_CALL.