Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_A
 zcl ias-ace a [armMode:1] [armDisarmCode:-1] [zoneId:1]
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_B
 zcl ias-ace b [numberOfZones:1] [zoneIds:1] [armDisarmCode:-1]
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_E
 zcl ias-ace e
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_F
 zcl ias-ace f
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_P
 zcl ias-ace p
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_GETZM
 zcl ias-ace getzm
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_GETZI
 zcl ias-ace getzi [zoneId:1]

Detailed Description

This group describes the CLI commands for the IAS ACE cluster. Listed below is a description of the cluster:

Attributes and commands for IAS Ancillary Control Equipment.

Macro Definition Documentation

#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_A

zcl ias-ace a [armMode:1] [armDisarmCode:-1] [zoneId:1]

  • Command description for Arm
    • armMode - IasAceArmMode [ENUM8]
    • armDisarmCode - CHAR_STRING
    • zoneId - INT8U
      See also
      EmberAfIasAceArmMode
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_B

zcl ias-ace b [numberOfZones:1] [zoneIds:1] [armDisarmCode:-1]

  • Command description for Bypass
    • numberOfZones - INT8U
    • zoneIds - INT8U
    • armDisarmCode - CHAR_STRING
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_E

zcl ias-ace e

  • Command description for Emergency
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_F

zcl ias-ace f

  • Command description for Fire
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_GETZI

zcl ias-ace getzi [zoneId:1]

  • Command description for GetZoneInformation
    • zoneId - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_GETZM

zcl ias-ace getzm

  • Command description for GetZoneIdMap
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IAS_ACE_P

zcl ias-ace p

  • Command description for Panic