Cluster Commands: IAS Zone
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_I_A_S_ZONE_SC |
zcl ias-zone sc [zoneStatus:2] [extendedStatus:1] [zoneId:1] [delay:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_I_A_S_ZONE_ENROLL |
zcl ias-zone enroll [zoneType:2] [manufacturerCode:2] |
Detailed Description
This group describes the CLI commands for the IAS Zone cluster. Listed below is a description of the cluster:
Attributes and commands for IAS security zone devices.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_I_A_S_ZONE_ENROLL |
zcl ias-zone enroll [zoneType:2] [manufacturerCode:2]
- Command description for zoneEnrollRequest
- zoneType - IasZoneType [ENUM16]
- manufacturerCode - INT16U
- See also
- EmberAfIasZoneType
#define EMBER_AF_DOXYGEN_CLI_COMMAND_I_A_S_ZONE_SC |
zcl ias-zone sc [zoneStatus:2] [extendedStatus:1] [zoneId:1] [delay:2]
- Command description for zoneStatusChangeNotification
- zoneStatus - IasZoneStatus [BITMAP16]
- extendedStatus - BITMAP8
- zoneId - INT8U
- delay - INT16U