Cluster Commands: Identify
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF |
zcl identify off [endpoint:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON |
zcl identify on [endpoint:1] [time:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID |
zcl identify id [identifyTime:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY |
zcl identify query | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE |
zcl identify ez-mode [action:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER |
zcl identify trigger [effectId:1] [effectVariant:1] |
Detailed Description
This group describes the CLI commands for the Identify cluster. Listed below is a description of the cluster:
Attributes and commands for putting a device into Identification mode (e.g. flashing a light).
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE |
zcl identify ez-mode [action:1]
- Invoke EZMode on an Identify Server
- action - BITMAP8
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID |
zcl identify id [identifyTime:2]
- Command description for Identify
- identifyTime - INT16U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY |
zcl identify query
- Command description for IdentifyQuery
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER |
zcl identify trigger [effectId:1] [effectVariant:1]
- Command description for TriggerEffect
- effectId - IdentifyEffectIdentifier [ENUM8]
- effectVariant - IdentifyEffectVariant [ENUM8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF |
zcl identify off [endpoint:1]
- Writes the IdentifyTime attribute
- endpoint - INT8U - The endpoint on which to stop identifying
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON |
zcl identify on [endpoint:1] [time:2]
- Writes the IdentifyTime attribute
- endpoint - INT8U - The endpoint on the device which should begin identifying
- time - INT16U - The number of seconds to spend identifying