Cluster Commands: Level Control
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL |
zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE |
zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP |
zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP |
zcl level-control stop [optionMask:1] [optionOverride:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL |
zcl level-control o-mv-to-level [level:1] [transitionTime:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE |
zcl level-control o-move [moveMode:1] [rate:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP |
zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP |
zcl level-control o-stop |
Detailed Description
This group describes the CLI commands for the Level Control cluster. Listed below is a description of the cluster:
Attributes and commands for controlling devices that can be set to a level between fully 'On' and fully 'Off.'
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE |
zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1]
- Command description for Move
- moveMode - MoveMode [ENUM8]
- rate - INT8U
- optionMask - BITMAP8
- optionOverride - BITMAP8
- See also
- EmberAfMoveMode
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL |
zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
- Command description for MoveToLevel
- level - INT8U
- transitionTime - INT16U
- optionMask - BITMAP8
- optionOverride - BITMAP8
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE |
zcl level-control o-move [moveMode:1] [rate:1]
- Command description for MoveWithOnOff
- moveMode - MoveMode [ENUM8]
- rate - INT8U
- See also
- EmberAfMoveMode
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL |
zcl level-control o-mv-to-level [level:1] [transitionTime:2]
- Command description for MoveToLevelWithOnOff
- level - INT8U
- transitionTime - INT16U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP |
zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2]
- Command description for StepWithOnOff
- stepMode - StepMode [ENUM8]
- stepSize - INT8U
- transitionTime - INT16U
- See also
- EmberAfStepMode
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP |
zcl level-control o-stop
- Command description for StopWithOnOff
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP |
zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
- Command description for Step
- stepMode - StepMode [ENUM8]
- stepSize - INT8U
- transitionTime - INT16U
- optionMask - BITMAP8
- optionOverride - BITMAP8
- See also
- EmberAfStepMode
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP |
zcl level-control stop [optionMask:1] [optionOverride:1]
- Command description for Stop
- optionMask - BITMAP8
- optionOverride - BITMAP8