Cluster Commands: MFGLIB Cluster
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_STREAM |
zcl mfglib stream [channel:1] [power:1] [time:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_TONE |
zcl mfglib tone [channel:1] [power:1] [time:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_RX_MODE |
zcl mfglib rx-mode [channel:1] [power:1] [time:2] |
Detailed Description
This group describes the CLI commands for the MFGLIB Cluster cluster. Listed below is a description of the cluster:
This cluster provides commands to kick off MFGLIB actions over the air.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_RX_MODE |
zcl mfglib rx-mode [channel:1] [power:1] [time:2]
- Command to put the device into RX mode.
- channel - INT8U
- power - INT8S
- time - INT16U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_STREAM |
zcl mfglib stream [channel:1] [power:1] [time:2]
- Command to put the device into streaming mode.
- channel - INT8U
- power - INT8S
- time - INT16U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_TONE |
zcl mfglib tone [channel:1] [power:1] [time:2]
- Command to put the device into tone mode.
- channel - INT8U
- power - INT8S
- time - INT16U