Plugin Commands: Calendar Client
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_CLEAR |
plugin calendar-client clear [endpoint:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_PRINT |
plugin calendar-client print [endpoint:1] |
Detailed Description
The Calendar Client plugin contributes several commands to the application framework's CLI. These commands are used for interacting with calendars.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_CLEAR |
plugin calendar-client clear [endpoint:1]
- Clear the calendars.
- endpoint - INT8U - The endpoint.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_PRINT |
plugin calendar-client print [endpoint:1]
- Print the calendars.
- endpoint - INT8U - The endpoint.