Plugin Commands: Door Lock Server Cluster
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_APPLY_PIN |
plugin door-lock-server apply-pin [pin:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_APPLY_RFID |
plugin door-lock-server apply-rfid [rfid:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_CLOSE |
plugin door-lock-server close | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_LOCK |
plugin door-lock-server lock [userId:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_OPEN |
plugin door-lock-server open | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_STATUS |
plugin door-lock-server status | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_UNLOCK |
plugin door-lock-server unlock [userId:2] |
Detailed Description
Commands pertaining to the Silicon Labs Door Lock server cluster.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_APPLY_PIN |
plugin door-lock-server apply-pin [pin:-1]
- Simulate a PIN being entered into the door lock.
- pin - OCTET_STRING - The PIN to enter into the door lock.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_APPLY_RFID |
plugin door-lock-server apply-rfid [rfid:-1]
- Simulate an RFID device being brought within range of the door lock.
- rfid - OCTET_STRING - The identifier of the RFID device.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_CLOSE |
plugin door-lock-server close
- Close the door (on currently hardcoded endpoint 1).
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_LOCK |
plugin door-lock-server lock [userId:2]
- Lock the door (on currently hardcoded endpoint 1).
- userId - INT16U - The user ID for whoever is locking the door.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_OPEN |
plugin door-lock-server open
- Open the door (on currently hardcoded endpoint 1).
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_STATUS |
plugin door-lock-server status
- Print out the current status of the door lock.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DOOR_LOCK_SERVER_PLUGIN_DOOR_LOCK_SERVER_UNLOCK |
plugin door-lock-server unlock [userId:2]
- Unlock the door (on currently hardcoded endpoint 1).
- userId - INT16U - The user ID for whoever is unlocking the door.