Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_GROUP_SINK
plugin green-power-client add-group-sink [sourceID:4] [sinkGroup:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_SINK
plugin green-power-client add-sink [sourceID:4] [sinkIeee:8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_CLEAR_PROXY_TABLE
plugin green-power-client clear-proxy-table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_DUPLICATE_FILTER_TEST
plugin green-power-client duplicate-filter-test [endpoint:1] [sourceId:4] [sequenceNumber:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_PRINT_PROXY_TABLE
plugin green-power-client print-proxy-table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_GPD
plugin green-power-client rm-gpd [sourceID:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_SINK
plugin green-power-client rm-sink [sourceID:4] [sinkIeee:8]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_KEY
plugin green-power-client set-key [index:1] [key:16]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_PROXY_ENTRY
plugin green-power-client set-proxy-entry [index:1] [sourceID:4] [sinkNodeId:2] [options:4]

Detailed Description

The Green Power Client plugin contributes CLI commands to the application framework to be used for getting, setting, and displaying information relevant to the Green Power Client cluster.

Macro Definition Documentation

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_GROUP_SINK

plugin green-power-client add-group-sink [sourceID:4] [sinkGroup:2]

  • Add a groupcast sink for a given GPD
    • sourceID - INT32U - GPD Source ID
    • sinkGroup - INT16U - Sink group
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_SINK

plugin green-power-client add-sink [sourceID:4] [sinkIeee:8]

  • Add a sink for a given GPD
    • sourceID - INT32U - GPD Source ID
    • sinkIeee - IEEE_ADDRESS - Sink's IEEE address
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_CLEAR_PROXY_TABLE

plugin green-power-client clear-proxy-table

  • clear the proxy table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_DUPLICATE_FILTER_TEST

plugin green-power-client duplicate-filter-test [endpoint:1] [sourceId:4] [sequenceNumber:1]

  • This is used to instrument the current device receiving a message in order to test the duplicate message filtering functionality.
    • endpoint - INT8U
    • sourceId - INT32U - source Id of the fake incoming message
    • sequenceNumber - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_PRINT_PROXY_TABLE

plugin green-power-client print-proxy-table

  • Print the proxy table
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_GPD

plugin green-power-client rm-gpd [sourceID:4]

  • Remove a given GPD from the proxy table
    • sourceID - INT32U - GPD Source ID
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_SINK

plugin green-power-client rm-sink [sourceID:4] [sinkIeee:8]

  • remove a sink for a given GPD. If that's the last sink, remove the proxy table entry
    • sourceID - INT32U - GPD Source ID
    • sinkIeee - IEEE_ADDRESS - Sink's IEEE address
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_KEY

plugin green-power-client set-key [index:1] [key:16]

  • This is used to set the key for a proxy table entry
    • index - INT8U
    • key - SECURITY_KEY - source Id of the fake incoming message
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_PROXY_ENTRY

plugin green-power-client set-proxy-entry [index:1] [sourceID:4] [sinkNodeId:2] [options:4]

  • Set a proxy table entry
    • index - INT8U - index to proxy table
    • sourceID - INT32U - GPD Source ID
    • sinkNodeId - INT16U - Sink's node address
    • options - INT32U