Plugin Commands: Multi-Network Price Passthrough
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_PRINT |
plugin mn-price-passthrough print | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_SET_ROUTING |
plugin mn-price-passthrough set-routing [fwdId:2] [fwdEndpoint:1] [esiEndpoint:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_START |
plugin mn-price-passthrough start | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_STOP |
plugin mn-price-passthrough stop |
Detailed Description
The Multi-Network Price Passthrough plugin is a plugin designed to demonstrate multi-network functionality by passing data from a "real" ESI on one network to a "proxy" ESI on another network via periodic polling and forwarding.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_PRINT |
plugin mn-price-passthrough print
- Print the current price known to the proxy esi.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_SET_ROUTING |
plugin mn-price-passthrough set-routing [fwdId:2] [fwdEndpoint:1] [esiEndpoint:1]
- Set the routing parameters.
- fwdId - INT16U - The node id of the forwarding endpoint.
- fwdEndpoint - INT8U - The forwarding endpoint.
- esiEndpoint - INT8U - The endpoint of the proxy ESI.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_START |
plugin mn-price-passthrough start
- Starts polling and forwarding.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_STOP |
plugin mn-price-passthrough stop
- Stops polling and forwarding.