Plugin Commands: Slot Manager
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_BOOT_SLOT |
plugin slot-manager boot-slot [slotId:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_ERASE_SLOT |
plugin slot-manager erase-slot [slotId:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_EXT_FLASH_INFO |
plugin slot-manager ext-flash-info | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_READ |
plugin slot-manager read [address:4] [length:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_SLOTS_INFO |
plugin slot-manager slots-info |
Detailed Description
This plugin provides a set of CLI commands to interact with external SPI flash, particularly in a setup where slots are present to work with the common bootloader.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_BOOT_SLOT |
plugin slot-manager boot-slot [slotId:4]
- Boot the image in the specified slot ID.
- slotId - INT32U - The slot ID to boot
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_ERASE_SLOT |
plugin slot-manager erase-slot [slotId:4]
- Erase the specified slot ID.
- slotId - INT32U - The slot ID to erase
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_EXT_FLASH_INFO |
plugin slot-manager ext-flash-info
- Print external flash information.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_READ |
plugin slot-manager read [address:4] [length:1]
- Read raw data from external flash.
- address - INT32U - Address to read
- length - INT8U - Length of bytes to read
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_SLOTS_INFO |
plugin slot-manager slots-info
- Print information for all available slots.