Plugin Commands: Tunneling Client
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_CLOSE |
plugin tunneling-client close [tunnelIndex:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_PRINT |
plugin tunneling-client print | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_REQUEST |
plugin tunneling-client request [server:2] [clientEndpoint:1] [serverEndpoint:1] [protocolId:1] [manufacturerCode:2] [flowControlSupport:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_TRANSFER |
plugin tunneling-client transfer [tunnelIndex:1] [data:-1] |
Detailed Description
The Tunneling Client Plugin contributes several commands to the application framework's CLI. These commands may be used to create messages related to opening and closing a tunnel between two devices.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_CLOSE |
plugin tunneling-client close [tunnelIndex:1]
- Close a Tunneling cluster tunnel.
- tunnelIndex - INT8U - The index of the tunnel to close.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_PRINT |
plugin tunneling-client print
- Print out the status of active tunnels.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_REQUEST |
plugin tunneling-client request [server:2] [clientEndpoint:1] [serverEndpoint:1] [protocolId:1] [manufacturerCode:2] [flowControlSupport:1]
- Request a Tunneling cluster tunnel with a server.
- server - INT16U - The network address of the server to which the request will be sent.
- clientEndpoint - INT8U - The local endpoint from which the request will be sent.
- serverEndpoint - INT8U - The remote endpoint to which the request will be sent.
- protocolId - INT8U - The protocol id of the requested tunnel.
- manufacturerCode - INT16U - The manufacturer code of the requested tunnel.
- flowControlSupport - BOOLEAN - 1 if flow control support is requested or 0 if not.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_TRANSFER |
plugin tunneling-client transfer [tunnelIndex:1] [data:-1]
- Transfer data to a server through a Tunneling cluster tunnel.
- tunnelIndex - INT8U - The index of the tunnel through which to send the data.
- data - OCTET_STRING - The data to send through the tunnel.