Plugin Commands: Update TC Link Key
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_UPDATE_TC_LINK_KEY_PLUGIN_UPDATE_TC_LINK_KEY_TIMER |
plugin update-tc-link-key timer [timeInMilliseconds:4] |
Detailed Description
The update trust center link key commands are used to manipulate the behavior of the joining device to attempt the trust center link key updates in a certain fashion.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_UPDATE_TC_LINK_KEY_PLUGIN_UPDATE_TC_LINK_KEY_TIMER |
plugin update-tc-link-key timer [timeInMilliseconds:4]
- This sets the the amount of time between subsequent trust center link key updates in milliseconds.
- timeInMilliseconds - INT32U - The amount of time between subsequent trust center link key updates in milliseconds