Cluster Commands: Scenes
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_ADD |
zcl scenes add [groupId:2] [sceneId:1] [transitionTime:2] [sceneName:-1] [extensionFieldSets:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_VIEW |
zcl scenes view [groupId:2] [sceneId:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_REMOVE |
zcl scenes remove [groupId:2] [sceneId:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_RMALL |
zcl scenes rmall [groupId:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_STORE |
zcl scenes store [groupId:2] [sceneId:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_RECALL |
zcl scenes recall [groupId:2] [sceneId:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_GET |
zcl scenes get [groupId:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_EADD |
zcl scenes eadd [groupId:2] [sceneId:1] [transitionTime:2] [sceneName:-1] [extensionFieldSets:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_EVIEW |
zcl scenes eview [groupId:2] [sceneId:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_COPY |
zcl scenes copy [mode:1] [groupIdFrom:2] [sceneIdFrom:1] [groupIdTo:2] [sceneIdTo:1] |
Detailed Description
This group describes the CLI commands for the Scenes cluster. Listed below is a description of the cluster:
Attributes and commands for scene configuration and manipulation.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_ADD |
zcl scenes add [groupId:2] [sceneId:1] [transitionTime:2] [sceneName:-1] [extensionFieldSets:4]
- Add a scene to the scene table. Extension field sets are supported, and are inputed as arrays of the form [[cluster ID] [length] [value0...n] ...]
- groupId - INT16U
- sceneId - INT8U
- transitionTime - INT16U
- sceneName - CHAR_STRING
- extensionFieldSets - struct SceneExtensionFieldSet
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_COPY |
zcl scenes copy [mode:1] [groupIdFrom:2] [sceneIdFrom:1] [groupIdTo:2] [sceneIdTo:1]
- Command description for CopyScene
- mode - ScenesCopyMode [BITMAP8]
- groupIdFrom - INT16U
- sceneIdFrom - INT8U
- groupIdTo - INT16U
- sceneIdTo - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_EADD |
zcl scenes eadd [groupId:2] [sceneId:1] [transitionTime:2] [sceneName:-1] [extensionFieldSets:4]
- Command description for EnhancedAddScene
- groupId - INT16U
- sceneId - INT8U
- transitionTime - INT16U
- sceneName - CHAR_STRING
- extensionFieldSets - struct SceneExtensionFieldSet
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_EVIEW |
zcl scenes eview [groupId:2] [sceneId:1]
- Command description for EnhancedViewScene
- groupId - INT16U
- sceneId - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_GET |
zcl scenes get [groupId:2]
- Command description for GetSceneMembership
- groupId - INT16U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_RECALL |
zcl scenes recall [groupId:2] [sceneId:1]
- Command description for RecallScene
- groupId - INT16U
- sceneId - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_REMOVE |
zcl scenes remove [groupId:2] [sceneId:1]
- Command description for RemoveScene
- groupId - INT16U
- sceneId - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_RMALL |
zcl scenes rmall [groupId:2]
- Command description for RemoveAllScenes
- groupId - INT16U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_STORE |
zcl scenes store [groupId:2] [sceneId:1]
- Command description for StoreScene
- groupId - INT16U
- sceneId - INT8U
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SCENES_VIEW |
zcl scenes view [groupId:2] [sceneId:1]
- Command description for ViewScene
- groupId - INT16U
- sceneId - INT8U