//API Reference //Commands & Events //L2CAP Connection Oriented Channels //sl_bt_evt_l2cap_command_rejected You are viewing ... The Bluetooth connection handle on which the event is received
// Bluetooth LE//Version 5.0 //API Reference ... To use these new events, the application needs to include the bluetooth_feature_legacy_scanner or bluetooth_feature_extended_scanner component.
Training ... // Bluetooth LE//Version 5.0 //API Reference //Commands & Events //Scanner ... You are viewing documentation for version: 5.0 sl_bt_evt_scanner_legacy_advertisement_reportScanner#
For legacy devices (BLExxx) <=1.5.0 4.0 ... Bluetooth 4.2 specifies the PHY bitrate to be exactly 1 Mbps. Bluetooth 5 (introduced in Bluetooth SDK v2.3) specifies PHY bitrates as follows:
0: Bonding request does not need to be confirmed ... Error code otherwise. Events sl_bt_evt_connection_parameters - Triggered after ... [in] connection Connection handle uint8_t
0 dBm is enough to cover about 10 to 15 m range, based on tests made with iBeacon example and Android ... events app_assert_status(sc); // Start general advertising and enable connections.