EmberAfAttributeMinMaxValue Struct Reference
Type describing the attribute default, min and max values.
#include <
af-types.h
>
Data Fields | |
EmberAfDefaultAttributeValue | defaultValue |
EmberAfDefaultAttributeValue | minValue |
EmberAfDefaultAttributeValue | maxValue |
Type describing the attribute default, min and max values.
This struct is required if the attribute mask specifies that this attribute has a known min and max values.
Field Documentation
EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::defaultValue |
Default value of the attribute.
EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::maxValue |
Maximum allowed value.
EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::minValue |
Minimum allowed value
The documentation for this struct was generated from the following file:
af-types.h