A struct containing endpoint information about a device.

#include <af-types.h>

Data Fields

EmberEUI64 eui64
 
EmberAfEndpointInfoStruct endpoints [EMBER_AF_MAX_ENDPOINTS_PER_DEVICE]
 
EmberAfDeviceDiscoveryStatus status
 
uint8_t discoveryFailures
 
uint8_t capabilities
 
uint8_t endpointCount
 
uint8_t stackRevision

A struct containing endpoint information about a device.

Field Documentation

uint8_t EmberAfDeviceInfo::capabilities
uint8_t EmberAfDeviceInfo::discoveryFailures
uint8_t EmberAfDeviceInfo::endpointCount
EmberEUI64 EmberAfDeviceInfo::eui64
uint8_t EmberAfDeviceInfo::stackRevision
EmberAfDeviceDiscoveryStatus EmberAfDeviceInfo::status

The documentation for this struct was generated from the following file:
  • af-types.h