EmberAfDeviceManagementCIN Struct Reference
#include <
af-types.h
>
Data Fields | |
uint8_t | cin [EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH+1] |
uint32_t | implementationDateTime |
uint32_t | issuerEventId |
Field Documentation
uint8_t EmberAfDeviceManagementCIN::cin[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH+1] |
uint32_t EmberAfDeviceManagementCIN::implementationDateTime |
uint32_t EmberAfDeviceManagementCIN::issuerEventId |
The documentation for this struct was generated from the following file:
af-types.h