EmberAfDeviceManagementPassword Struct Reference
#include <
af-types.h
>
Data Fields | |
uint8_t | password [EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH+1] |
uint32_t | implementationDateTime |
uint16_t | durationInMinutes |
EmberAfDeviceManagementPasswordType | passwordType |
Field Documentation
uint16_t EmberAfDeviceManagementPassword::durationInMinutes |
uint32_t EmberAfDeviceManagementPassword::implementationDateTime |
uint8_t EmberAfDeviceManagementPassword::password[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH+1] |
EmberAfDeviceManagementPasswordType EmberAfDeviceManagementPassword::passwordType |
The documentation for this struct was generated from the following file:
af-types.h