EmberAfDeviceManagementSiteId Struct Reference
#include <
af-types.h
>
Data Fields | |
uint8_t | siteId [EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH+1] |
uint32_t | implementationDateTime |
uint32_t | issuerEventId |
Field Documentation
uint32_t EmberAfDeviceManagementSiteId::implementationDateTime |
uint32_t EmberAfDeviceManagementSiteId::issuerEventId |
uint8_t EmberAfDeviceManagementSiteId::siteId[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH+1] |
The documentation for this struct was generated from the following file:
af-types.h