EmberAfDeviceManagementSupplier Struct Reference

#include <af-types.h>

Data Fields

uint32_t proposedProviderId
 
uint32_t implementationDateTime
 
uint32_t providerChangeControl
 
uint8_t proposedProviderName [EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH+1]
 
uint8_t proposedProviderContactDetails [EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH+1]

Field Documentation

uint32_t EmberAfDeviceManagementSupplier::implementationDateTime
uint8_t EmberAfDeviceManagementSupplier::proposedProviderContactDetails[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH+1]
uint32_t EmberAfDeviceManagementSupplier::proposedProviderId
uint8_t EmberAfDeviceManagementSupplier::proposedProviderName[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH+1]
uint32_t EmberAfDeviceManagementSupplier::providerChangeControl

The documentation for this struct was generated from the following file:
  • af-types.h