EmberAfDeviceManagementTenancy Struct Reference
#include <
af-types.h
>
Data Fields | |
uint32_t | providerId |
uint32_t | issuerEventId |
uint8_t | tariffType |
uint32_t | implementationDateTime |
uint32_t | tenancy |
Field Documentation
uint32_t EmberAfDeviceManagementTenancy::implementationDateTime |
uint32_t EmberAfDeviceManagementTenancy::issuerEventId |
uint32_t EmberAfDeviceManagementTenancy::providerId |
uint8_t EmberAfDeviceManagementTenancy::tariffType |
uint32_t EmberAfDeviceManagementTenancy::tenancy |
The documentation for this struct was generated from the following file:
af-types.h