EmberAfOtaImageId Struct Reference
This is a unique identifier for referencing zigbee Over-the-air upgrade images. It is used by the OTA plugins when passing around information about an upgrade file.
#include <
af-types.h
>
Data Fields | |
uint16_t | manufacturerId |
uint16_t | imageTypeId |
uint32_t | firmwareVersion |
uint8_t | deviceSpecificFileEui64 [EUI64_SIZE] |
This is a unique identifier for referencing zigbee Over-the-air upgrade images. It is used by the OTA plugins when passing around information about an upgrade file.
Field Documentation
uint8_t EmberAfOtaImageId::deviceSpecificFileEui64[EUI64_SIZE] |
This is only used for device specific files. It will be set to all 0's when the image does not have an upgrade destination field in it. Little endian format.
uint32_t EmberAfOtaImageId::firmwareVersion |
uint16_t EmberAfOtaImageId::imageTypeId |
uint16_t EmberAfOtaImageId::manufacturerId |
The documentation for this struct was generated from the following file:
af-types.h