A structure used to store scene table entries in RAM or in tokens, depending on a plugin setting. If endpoint field is EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID, the entry is unused.
#include <af-types.h
>
A structure used to store scene table entries in RAM or in tokens, depending on a plugin setting. If endpoint field is EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID, the entry is unused.
uint8_t EmberAfSceneTableEntry::endpoint |
uint16_t EmberAfSceneTableEntry::groupId |
uint8_t EmberAfSceneTableEntry::sceneId |
uint16_t EmberAfSceneTableEntry::transitionTime |
uint8_t EmberAfSceneTableEntry::transitionTime100ms |
The documentation for this struct was generated from the following file: