EmberNetworkInitStruct Struct Reference
Defines the network initialization configuration that should be used when ::emberNetworkInit() is called by the application.
#include <
ember-types.h
>
Data Fields | |
EmberNetworkInitBitmask | bitmask |
Defines the network initialization configuration that should be used when ::emberNetworkInit() is called by the application.
Field Documentation
EmberNetworkInitBitmask EmberNetworkInitStruct::bitmask |
The documentation for this struct was generated from the following file:
ember-types.h