EmberSmacData Struct Reference

This data structure contains the Shared Message Authentication Code (SMAC) data that is used for Certificate Based Key Exchange (CBKE).

#include <ember-types.h>

Data Fields

uint8_t contents [EMBER_SMAC_SIZE]

This data structure contains the Shared Message Authentication Code (SMAC) data that is used for Certificate Based Key Exchange (CBKE).

Field Documentation

uint8_t EmberSmacData::contents[EMBER_SMAC_SIZE]

The documentation for this struct was generated from the following file:
  • ember-types.h