EmberVersion Struct Reference

A version structure containing all version information.

#include <ember-types.h>

Data Fields

uint16_t build
 
uint8_t major
 
uint8_t minor
 
uint8_t patch
 
uint8_t special
 
EmberVersionType type

A version structure containing all version information.

Field Documentation

uint16_t EmberVersion::build
uint8_t EmberVersion::major
uint8_t EmberVersion::minor
uint8_t EmberVersion::patch
uint8_t EmberVersion::special
EmberVersionType EmberVersion::type

The documentation for this struct was generated from the following file:
  • ember-types.h