// Bluetooth LE//Version 5.0 //API Reference ... _report and sl_bt_evt_scanner_extended_advertisement_report events Data Structures struct ... Value 0 indicates no periodic advertising.
// Bluetooth LE//Version 5.0 //API Reference ... Bits 0 - 2: Highest 3 bits of the data payload length field Bits 3 - 5: Device type Bit value 100: Bluetooth LE Bit value 101: Bluetooth Mesh
0: Bonding request does not need to be confirmed ... Data includes remote device address and address type as well as security mode for ... address The Bluetooth device address uint32_t *
// Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System ... Bluetooth identity address in little endian format ... data Data to write Write data into the system data buffer.
Bluetooth API is incorrect on EFR32M|B1, EFR32M|B12, EFR32M|B13, and EFR32M|B21 ... Data polls from forgotten end device children were not properly setting a pending frame ... 1334477 7.5 None