Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS writes the file to extended flash or bulk flash, depending on the location option: -l extended/bulk . ... [Disassociated] SILABS-WGM160P-4.0.0, Gecko_OS-STANDARD-4.0.12-1198, WGM160P
os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren ) ... stream mode, either with the str_select GPIO (see gfu ), or by issuing the the str ...
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for zigbee/6.4/group-plugin-messaging-client