Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... reboot ... wlan.scan.num_probes wlan.scan.passive_dwell wlan.scan.retries wlan.scan.type
ProductWirelessResource TypeSoftware API documentation
Command data types. ... Issue Gecko OS command, return result data in buffer. ... fmt Formatted Gecko OS command Returns gos_result_t result of api call ◆ gos_cmd_issue_with_callback()
ProductWirelessResource TypeSoftware API documentation
os pins can only use the strong drive strength. ... Scan intervals and configuration are defined by ce s h d , ce s h i , ce s l d , and ce s ... scan accepts an optional <threshold> argument.
ProductWirelessResource TypeSoftware API documentation
wlan_get_rssi wlan_scan GPIOs and Peripherals ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... t ype: specify file type as integer or hex string 2 .
Results 1-5 of 5 for zigbee/6.4/structEmberAfDeviceManagementTenancy