Ember Application Framework Command Line Interface (CLI)
Macros | |
#define | EMBER_AF_DOXYGEN_CLI__NETWORK_COMMANDS |
network form <channel> <power> <panid> | |
#define | EMBER_AF_DOXYGEN_CLI__SECURITY_CHANGEKEY_COMMANDS |
Commands used to change the default link or network key that will be used when forming or joining a network. | |
#define | EMBER_AF_DOXYGEN_CLI__SECURITY_CBKE_COMMANDS |
Command used for key establishment. | |
#define | EMBER_AF_DOXYGEN_CLI__ZCL_GLOBAL_COMMANDS |
Commands used to send global commands in the zcl. |
Detailed Description
This header provides cli command function prototypes for the Application Framework's core ZigBee Cluster Library implementation.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI__NETWORK_COMMANDS |
network form <channel> <power> <panid>
- Form a network on a given channel, with a given TX Power and PAN ID.
- channel - uint8_t. The channel on which to form the network.
- power - int8_t. One byte signed value indicating the TX Power that the radio should be set to.
- panId - uint16_t. The PAN ID on which to form the network.
network join <channel> <power> <panid>
- Join a network on a given channel, with a given TX Power and PAN ID.
- channel - uint8_t. The channel on which to join the network.
- power - int8_t. One byte signed value indicating the TX Power that the radio should be set to.
- panId - uint16_t. The PAN ID on which to join the network.
network rejoin <encrypted>
- Find and rejoin the previous network the device was connected to.
- encrypted - uint8_t. A single byte boolean 0 or 1 indicating whether or not the rejoin should be done with encryption.
network leave
- Leave the current network that the device is connected to.
network pjoin <seconds>
- Turn permit joining on for the amount of time indicated.
- seconds - uint8_t. A single byte indicating how long the device should have permit joining turn on for. A value of 0xff turns permit join indefinitely.
network broad-pjoin <seconds>
- Turn permit joining on for the amount of time indicated AND broadcast a ZDO Mgmt Permit Joining request to all routers.
- seconds - uint8_t. A single byte indicating how long the device should have permit joining turn on for. A value of 0xff turns permit join indefinitely.
network extpanid <bytes>
- Write the extended PAN ID of the device.
- bytes - byte array. An array of bytes which represents the extended PAN ID for the device.
network find unused
- Begins a search for an unused Channel and PAN ID. Will automatically form a network on the first unused Channel and PAN ID it finds.
network find joinable
- Begins a search for a joinable network. Will automatically attempt to join the first network it finds.
#define EMBER_AF_DOXYGEN_CLI__SECURITY_CBKE_COMMANDS |
Command used for key establishment.
cbke start <new partner id> <destination endpoint>
- new partner ID - uint16_t. The 2 byte node ID of the partner with whom to start cbke.
cbke interpan <pan id> <eui64>
- PAN ID - uint16_t. The 2 byte PAN ID that the target is located on.
- eui64 - EmberEUI64. The 8 byte EUI64 of the target (big endian)
cbke partner <node id> <endpoint>
- node ID - uint16_t. The two byte node ID of the device with whom to initiate key establishment.
- endpoint - uint8_t. The endpoint on which to begin key establishment.
#define EMBER_AF_DOXYGEN_CLI__SECURITY_CHANGEKEY_COMMANDS |
Commands used to change the default link or network key that will be used when forming or joining a network.
changekey link <key>
- key - 16 byte array. The Link Key provided as a 16 byte array.
changekey network <key>
- key - 16 byte array. The Network Key provided as a 16 byte array.
#define EMBER_AF_DOXYGEN_CLI__ZCL_GLOBAL_COMMANDS |
Commands used to send global commands in the zcl.
zcl global read <cluster> <attribute id>
- Creates a global read command message to read from the cluster and attribute specified.
- cluster - uint16_t. The cluster id to read from.
- attribute id - uint16_t. The attribute id to read from
zcl global write <cluster> <attribute id> <data type> <data>
- Creates a global write command message to write to the cluster and attribute specified.
- cluster - uint16_t. The cluster id to read from.
- attribute id - uint16_t. The attribute id to read from
- data type - uint8_t. The two byte zigbee type value
- data - byte array. The data to write
zcl global uwrite <cluster> <attribute id> <data type> <data>
- Creates a global write command message to write to the cluster and attribute specified.
- cluster - uint16_t. The cluster id to read from.
- attribute id - uint16_t. The attribute id to read from
- data type - uint8_t. The two byte zigbee type value
- data - byte array. The data to write
zcl global nwrite <cluster> <attribute id> <data type> <data>
- Creates a global write command message to write to the cluster and attribute specified.
- cluster - uint16_t. The cluster id to read from.
- attribute id - uint16_t. The attribute id to read from
- data type - uint8_t. The two byte zigbee type value
- data - byte array. The data to write
zcl global discover <cluster> <attribute id> <max>
- Creates discovery message for devices with the associated cluster and attribute
- cluster - uint16_t. The cluster id to read from.
- attribute id - uint16_t. The attribute id to read from
- max - uint8_t. Max number of discovery responses.
zcl global report-read <cluster> <attribute id> <direction>
- Creates a global read reporting command for the associated cluster, attribute and server/client direction.
- cluster - uint16_t. The cluster id to read from.
- attribute id - uint16_t. The attribute id to read from
- direction - uint8_t. 0 for client-to-server, 1 for server-to-client.
zcl global send-me-a-report <cluster> <attribute id> <data type> <min report time> <max report time> <reportable change>
- Creates a global send me a report command for the associated values.
- cluster - uint16_t. The cluster id for requested report.
- attribute id - uint16_t. The attribute for requested report.
- data type - uint8_t. The two byte zigbee type value for the requested report
- min report time - uint16_t. Minimum number of seconds between reports.
- max report time - uint16_t. Maximum number of seconds between reports.
- reportable change - byte array. Amount of change to trigger a report.
zcl global expect-report-from-me <cluster> <attribute id> <timeout>
- Create a expect-report-from-me message with associated values.
- cluster - uint16_t. The cluster id for requested report.
- attribute id - uint16_t. The attribute for requested report.
- timeout - uint16_t. The maximum amount of time between reports.
zcl global direction <direction>
- Sets the direction for global commands, either client to server or server to client.
- direction - uint8_t. The direction for global commands. client-to-server == 0, server-to-client == 1.
zcl global disc-com-gen <start command id> <max command ids>
- Sends a global Discover Commands Generated command.
- start command id - uint8_t. The command id to start discovery at.
- max command ids - uint8_t. The maximum number of command ids to return.
zcl global disc-com-rec <start command id> <max command ids>
- Sends a global Discover Commands Received command.
- start command id - uint8_t. The command id to start discovery at.
- max command ids - uint8_t. The maximum number of command ids to return.