Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ECHO |
echo [echoOn:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_EVENTS |
events | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_RESET |
reset | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_MFG_CODE |
zcl mfg-code [mfgSpecificId:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_TIME |
zcl time [utcTime:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_USE_NEXT_SEQUENCE |
zcl use-next-sequence [useNextSequence:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_X_DEFAULT_RESP |
zcl x-default-resp [disableDefaultResponse:1] |
Detailed Description
General commands that are applicable to the node regardless of clusters or plugins.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ECHO |
echo [echoOn:1]
- Turns echo on the command line on or off depending on the argument
- echoOn - INT8U - bool indicating whether to turn echo on (1) or off (0)
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_EVENTS |
events
- Print the list of timer events.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_RESET |
reset
- resets the device
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_MFG_CODE |
zcl mfg-code [mfgSpecificId:2]
- Sets the two byte manufacturer specific identifier to use for the next command if the command is not already built.
- mfgSpecificId - INT16U - Manufacturer Specific Id
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_TIME |
zcl time [utcTime:4]
- Cli command to call emberAfSetTime function documented in
af.h
- utcTime - INT32U - ZigBee UTC time, number of seconds since the year 2000
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_USE_NEXT_SEQUENCE |
zcl use-next-sequence [useNextSequence:1]
- Sets the flag to use the incremented sequence number from the framework for the next raw command.
- useNextSequence - BOOLEAN - bool value indicating whether raw command will use the incremented seq number from framework, set(1) or not(0).
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERAL_ZCL_X_DEFAULT_RESP |
zcl x-default-resp [disableDefaultResponse:1]
- Sets the Disable Default Response Frame Control bit to use for the next command if the command is not already built.
- disableDefaultResponse - BOOLEAN - bool value indicating whether the disable default response bit is set(1) or not (0).