GPIO Sensor Interface Callbacks
Functions | |
void | emberAfPluginGpioSensorStateChangedCallback (uint8_t newSensorState) |
Called whenever the GPIO sensor detects a change in state. |
Detailed Description
These callbacks are contributed by the GPIO Sensor Interface plugin.
Function Documentation
void emberAfPluginGpioSensorStateChangedCallback | ( | uint8_t | newSensorState | ) |
Called whenever the GPIO sensor detects a change in state.
- Parameters
-
newSensorState
The new state of the sensor based alarm (EMBER_AF_PLUGIN_GPIO_SENSOR_ACTIVE or EMBER_AF_PLUGIN_GPIO_SENSOR_NOT_ACTIVE) Ver.: always