Plugin Commands: Concentrator
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_AGG |
plugin concentrator agg | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_HOST_TABLE |
plugin concentrator print-host-table | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_TABLE |
plugin concentrator print-table | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_SET_ROUTER_BEHAVIOR |
plugin concentrator set-router-behavior [behavior:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_START |
plugin concentrator start | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STATUS |
plugin concentrator status | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STOP |
plugin concentrator stop |
Detailed Description
The Concentrator plugin contributes several CLI commands to the application framework for controlling the sending of MTORRs.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_AGG |
plugin concentrator agg
- (Requires Concentrator Support to be enabled on this device.) Schedules a ZigBee PRO Many To One Route Request (MTORR) to be sent out at next opportunity, which will cause aggregation (many-to-one) routes to be created towards this concentrator.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_HOST_TABLE |
plugin concentrator print-host-table
- Print the host source route table.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_TABLE |
plugin concentrator print-table
- Print the SOC/NCP source route table.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_SET_ROUTER_BEHAVIOR |
plugin concentrator set-router-behavior [behavior:1]
- This command allows the user to set the router behavior for this plugin. The argument values come from concentrator-support.h in the enum with members starting with EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_.
- behavior - INT8U - The value of a EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_ enum member.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_START |
plugin concentrator start
- Starts the periodic broadcast of MTORRs
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STATUS |
plugin concentrator status
- Prints current status and configured parameters of the concentrator
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STOP |
plugin concentrator stop
- Stops the periodic broadcast of MTORRs