Plugin Commands: Manufacturing Library
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_LOCK |
plugin configuration-server lock [lock:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_READ |
plugin configuration-server read | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_SET |
plugin configuration-server set [creator:2] [data:-1] |
Detailed Description
CLI commands related to the manufacturing library.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_LOCK |
plugin configuration-server lock [lock:1]
- Lock/unlock the configuration cluster.
- lock - BOOLEAN - True means lock, false means unlock.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_READ |
plugin configuration-server read
- Read a token supported by the configuration server.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_SET |
plugin configuration-server set [creator:2] [data:-1]
- Set a token supported by the configuration server.
- creator - INT16U - True means lock, false means unlock.
- data - OCTET_STRING - Data to use to write the token.