Plugin Commands: GBCS Device Log
Detailed Description
The gbcs-device-log plugin contributes several CLI commands to the application framework to be used in configuring and managing the GBCS Device Log.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_CLEAR |
plugin gbcs-device-log clear
- Clear all entries from the GBCS Device Log.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_COUNT |
plugin gbcs-device-log count
- Get the number of entries in the GBCS Device Log.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_EXISTS |
plugin gbcs-device-log exists [deviceId:8] [deviceType:1]
- Check to see if a device exists in the GBCS Device Log.
- deviceId - IEEE_ADDRESS - The EUI64 of the device in question
- deviceType - INT8U - The GBCS device type of the device in question
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_FILL |
plugin gbcs-device-log fill
- Helper command to fill the GBCS Device Log with random info.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_GET |
plugin gbcs-device-log get [deviceId:8]
- Get device info about an entry in the GBCS Device Log
- deviceId - IEEE_ADDRESS - The EUI64 of the device for which information is requested
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_IS_SLEEPY |
plugin gbcs-device-log is-sleepy [deviceType:1]
- Is the given device type a sleepy device.
- deviceType - INT8U - The GBCS device type to be checked
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_PRINT |
plugin gbcs-device-log print
- Print all entries in the GBCS Device log.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_REMOVE |
plugin gbcs-device-log remove [deviceId:8]
- Remove an entry from the GBCS Device Log.
- deviceId - IEEE_ADDRESS - The EUI64 of the device to be removed
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_RESET |
plugin gbcs-device-log reset
- Reset the GBCS Device Log to include just those entries configured with the plugin.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_STORE |
plugin gbcs-device-log store [deviceId:8] [deviceType:1]
- Add or update an entry within the GBCS Device Log.
- deviceId - IEEE_ADDRESS - The EUI64 of the device to be added or updated
- deviceType - INT8U - The GBCS device type of the device to be added or updated