Plugin Commands: IAS Zone Server
Detailed Description
This plugin provides a set of CLI commands for managing the local IAS Zone server.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_CHANGE_BACKOFF_CONFIG |
plugin ias-zone-server change-backoff-config [firstBackoff:1] [commonRatio:1] [maxBackoff:4] [unlimitedRetries:1] [maxRetryAttempts:2]
- Update the IAS Zone server's backoff configuration parameters.
- firstBackoff - INT8U - First backoff time in seconds.
- commonRatio - INT8U - Backoff increase common ratio.
- maxBackoff - INT32U - Maximum backoff time in seconds.
- unlimitedRetries - BOOLEAN - Unlimited retires.
- maxRetryAttempts - INT16U - Maximum retry attempts.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_CHANGE_STATUS |
plugin ias-zone-server changeStatus [newStatus:2] [timeSinceOccurredSeconds:1] [endpoint:1]
- Update the zone status attribute of a given endpoint's IAS Zone cluster to the given value
- newStatus - INT16U - The new status to be written
- timeSinceOccurredSeconds - INT8U - The amount time that has passed since the last update occurred (seconds)
- endpoint - INT8U - The endpoint whose zone status attribute is to be updated
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_INFO |
plugin ias-zone-server info [endpoint:1]
- Print current value of the following cluster attributes: zone type, zone state, zone status, zone id
- endpoint - INT8U - The endpoint whose IAS Zone Cluster information is to be printed
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_PRINT_QUEUE |
plugin ias-zone-server print-queue
- Prints information on the status queue.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_PRINT_QUEUE_CONFIG |
plugin ias-zone-server print-queue-config
- Prints the status queue config.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_SET_ENROLLMENT_MODE |
plugin ias-zone-server set-enrollment-mode [endpoint:1] [enrollmentMode:1]
- Update the IAS Zone server's enrollment method to the specified value
- endpoint - INT8U - The endpoint whose enrollment mode is to be updated
- enrollmentMode - INT8U - The new enrollment mode