Plugin Commands: Meter Mirror
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_MIRROR_PLUGIN_METER_MIRROR_REMOVE |
plugin meter-mirror remove [endpoint:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_MIRROR_PLUGIN_METER_MIRROR_STATUS |
plugin meter-mirror status |
Detailed Description
The Meter mirror plugin provides commands for managing the meter devices whose attributes are mirrorred locally.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_MIRROR_PLUGIN_METER_MIRROR_REMOVE |
plugin meter-mirror remove [endpoint:1]
- Manually removes a registered mirror at the specified endpoint.
- endpoint - INT8U - The endpoint of the mirror to remove.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_MIRROR_PLUGIN_METER_MIRROR_STATUS |
plugin meter-mirror status
- Prints the status of all mirrors.