Plugin Commands: Network Steering
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_ADD |
plugin network-steering mask add [whichMask:1] [channel:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SET |
plugin network-steering mask set [whichMask:1] [mask:4] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SUBTRACT |
plugin network-steering mask subtract [whichMask:1] [channel:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_START |
plugin network-steering start [options:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STATUS |
plugin network-steering status | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STOP |
plugin network-steering stop |
Detailed Description
The Network Steering plugin commands are currently being used for the Profile Interop event.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_ADD |
plugin network-steering mask add [whichMask:1] [channel:1]
- Adds a channel to either the primary or secondary channel mask of the network-steering plugin.
- whichMask - INT8U - The channel mask to add a channel to.
- channel - INT8U - The channel to add to the mask.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SET |
plugin network-steering mask set [whichMask:1] [mask:4]
- Set either the primary or secondary channel mask.
- whichMask - INT8U - The channel mask to subtract the channel from.
- mask - INT32U - The value to set the channel mask to.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SUBTRACT |
plugin network-steering mask subtract [whichMask:1] [channel:1]
- Subtracts a channel from either the primary or secondary channel mask of the network-steering plugin.
- whichMask - INT8U - The channel mask to subtract the channel from.
- channel - INT8U - The channel to subtract the mask from.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_START |
plugin network-steering start [options:1]
- Starts the network steering process.
- options - INT8U - A mask of options for indicating specific behavior within the network-steering process.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STATUS |
plugin network-steering status
- Displays the current status of the network steering process.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STOP |
plugin network-steering stop
- Stops the network steering process.