Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_DATA_PRINT
 plugin ota-storage-common data-print [index:1] [offset:4]
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_DELETE
 plugin ota-storage-common delete [index:1]
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_PRINT_IMAGES
 plugin ota-storage-common printImages
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_RELOAD
 plugin ota-storage-common reload
 
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_STORAGE_INFO
 plugin ota-storage-common storage-info

Detailed Description

The OTA Storage Common plugin provides Over-the-air commands for upgrading firmware and downloading specific files common to both server and client.

Macro Definition Documentation

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_DATA_PRINT

plugin ota-storage-common data-print [index:1] [offset:4]

  • Print arbitray bytes of the OTA image on disk.
    • index - INT8U - The index of the image to print its data.
    • offset - INT32U - The offset into the OTA image that will be printed.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_DELETE

plugin ota-storage-common delete [index:1]

  • Deletes the image at the specified index.
    • index - INT8U - The index at which to begin bootloading the image
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_PRINT_IMAGES

plugin ota-storage-common printImages

  • Prints the images.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_RELOAD

plugin ota-storage-common reload

  • Reload the storage device.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_STORAGE_INFO

plugin ota-storage-common storage-info

  • Print information about the storage device.