Plugin Commands: Trust Center Backup
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_CLEAR_IMPORT |
plugin trust-center-backup clear-import | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_IMPORT_KEY |
plugin trust-center-backup import-key [index:1] [partnerEUI64:8] [newKey:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_PRINT_EXPORT |
plugin trust-center-backup print-export | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_PRINT_IMPORT |
plugin trust-center-backup print-import | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_RESTORE |
plugin trust-center-backup restore | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_SET_EXT_PAN |
plugin trust-center-backup set-ext-pan [extendedPanId:8] |
Detailed Description
The Trust Center Backup plugin contributes several CLI commands to the application framework to be used in creating and managing reporting table entries directly on the device.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_CLEAR_IMPORT |
plugin trust-center-backup clear-import
- Clear the import data set.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_IMPORT_KEY |
plugin trust-center-backup import-key [index:1] [partnerEUI64:8] [newKey:-1]
- Set a key in the import data set.
- index - INT8U
- partnerEUI64 - IEEE_ADDRESS
- newKey - OCTET_STRING
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_PRINT_EXPORT |
plugin trust-center-backup print-export
- Print the set of export data that a TC must backup.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_PRINT_IMPORT |
plugin trust-center-backup print-import
- Print the import data set.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_RESTORE |
plugin trust-center-backup restore
- Use the import data set in a restore operation to bring the TC back online.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_SET_EXT_PAN |
plugin trust-center-backup set-ext-pan [extendedPanId:8]
- Set the extended PAN ID in the import data set.
- extendedPanId - IEEE_ADDRESS