Plugin Commands: Tunneling Server
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_SERVER_PLUGIN_TUNNELING_SERVER_BUSY |
plugin tunneling-server busy | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_SERVER_PLUGIN_TUNNELING_SERVER_PRINT |
plugin tunneling-server print | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_SERVER_PLUGIN_TUNNELING_SERVER_TRANSFER |
plugin tunneling-server transfer [tunnelIndex:2] [data:-1] |
Detailed Description
The Tunneling Server Plugin contributes several commands to the application framework CLI. These commands are used for the transfer of data over an opened tunnel.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_SERVER_PLUGIN_TUNNELING_SERVER_BUSY |
plugin tunneling-server busy
- This command can be used as a test harness for testing a client's handling of a server that returns busy.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_SERVER_PLUGIN_TUNNELING_SERVER_PRINT |
plugin tunneling-server print
- Print out the status of active tunnels.
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_SERVER_PLUGIN_TUNNELING_SERVER_TRANSFER |
plugin tunneling-server transfer [tunnelIndex:2] [data:-1]
- Transfer data to a client through a Tunneling cluster tunnel.
- tunnelIndex - INT16U - The identifier of the tunnel through which to send the data.
- data - OCTET_STRING - The data to send through the tunnel.