Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_CONF_MODE
plugin wwah-server confMode [mode:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_POWERING_OFF
plugin wwah-server poweringOff [srcEndpoint:1] [dstEndpoint:1] [reason:1] [mfgId:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_POWERING_ON
plugin wwah-server poweringOn [srcEndpoint:1] [dstEndpoint:1] [reason:1] [mfgId:2]

Detailed Description

The wwah-server plugin contributes CLI commands to the application framework to be used for printing information related to the WWAH server.

Macro Definition Documentation

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_CONF_MODE

plugin wwah-server confMode [mode:1]

  • Set the configurationModeEnabled attribute command.
    • mode - INT8U - The wwah server configuration mode attribute
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_POWERING_OFF

plugin wwah-server poweringOff [srcEndpoint:1] [dstEndpoint:1] [reason:1] [mfgId:2]

  • Send the Powering Off Notification command.
    • srcEndpoint - INT8U - The wwah server (source) endpoint
    • dstEndpoint - INT8U - The wwah client (dest) endpoint
    • reason - INT8U - The cause of the power off event
    • mfgId - INT16U - The manufacturerId of the sender
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_POWERING_ON

plugin wwah-server poweringOn [srcEndpoint:1] [dstEndpoint:1] [reason:1] [mfgId:2]

  • Send the Powering On Notification command.
    • srcEndpoint - INT8U - The wwah server (source) endpoint
    • dstEndpoint - INT8U - The wwah client (dest) endpoint
    • reason - INT8U - The cause of the power on event
    • mfgId - INT16U - The manufacturerId of the sender