EmberAfDeviceManagementCIN Struct Reference

#include <af-types.h>

Data Fields

uint8_t cin [EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH+1]
 
uint32_t implementationDateTime
 
uint32_t issuerEventId

Field Documentation

uint8_t EmberAfDeviceManagementCIN::cin[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH+1]
uint32_t EmberAfDeviceManagementCIN::implementationDateTime
uint32_t EmberAfDeviceManagementCIN::issuerEventId

The documentation for this struct was generated from the following file:
  • af-types.h