EmberAfDeviceManagementSiteId Struct Reference

#include < af-types.h >

Data Fields

uint8_t siteId [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH +1]
uint32_t implementationDateTime
uint32_t issuerEventId

Field Documentation

uint32_t EmberAfDeviceManagementSiteId::implementationDateTime
uint32_t EmberAfDeviceManagementSiteId::issuerEventId
uint8_t EmberAfDeviceManagementSiteId::siteId[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH +1]

The documentation for this struct was generated from the following file:
  • af-types.h