EmberAfDeviceManagementSupply Struct Reference
#include <
af-types.h
>
Data Fields | |
uint32_t | requestDateTime |
uint32_t | implementationDateTime |
uint8_t | supplyStatus |
uint8_t | originatorIdSupplyControlBits |
Field Documentation
uint32_t EmberAfDeviceManagementSupply::implementationDateTime |
uint8_t EmberAfDeviceManagementSupply::originatorIdSupplyControlBits |
uint32_t EmberAfDeviceManagementSupply::requestDateTime |
uint8_t EmberAfDeviceManagementSupply::supplyStatus |
The documentation for this struct was generated from the following file:
af-types.h